Post Go back to editing

FPGA design files for D2390A-A evaluation board and Arrow/Terasic SoCkit Cyclone V FPGA evaluation board

I am using the DC2390A-A evaluation board for the LTC2500-32 ADC with the Arrow/Terasic SoCkit Cyclone V FPGA evaluation board.  I cannot find the design files for the Arrow/Terasic SoCkit evaluation board for use with the DC2390A-A.  I am in need of the design files to program the Cyclone V FPGA of the SoCkit evaluation board so that I can evaluate the LTC2500-32 on the DC2390A-A evaluation board.

I can't even find the pinout information for the DC2390A-A evaluation board!  So at this point, the DC2390A-A evaluation board is useless.

Thank you for any assistance with this issue!

Parents Reply Children
  • python.zipI have uploaded a zipped file that you should download, unzip and overwrite the Python directory in your LinearLab Tools directory with. This should fix your problem.

  • I unfortunately obtain the same error message.  Python cannot find the "dc2390" module.  Neither can I.

  • The updated file was renamed  to DC2390_full_datapath_test_oldclient.py

    You will find it in the new Python directory in the llt\app_examples\ltc2500_family directory.

  • It appears that some progress has been made.  I am able to successfully run script "DC2390_full_datapath_test_oldclient.py", but the outputs are not meaningful and the message "Address out of range. Must be less than 0x100000" frequently appears as shown in the attached screenshot.

  • Also, the majority of the other scripts included in the "\linear_lab_tools64\python\llt\app_examples\ltc2500_family" directory do not run, while the few that do successfully run do not output meaningful information.  I can provide the associated screenshots if they are useful on your end.

    Thank you for your continued support!

  • When running DC2390_full_datapath_test_oldclient.py do you have the DC2390 DAC outputs connected to the ADC inputs?

  • Yes, as per the DC2390A Demo Manual.  And all jumpers are at their default positions.

  • Attached is the full output from the "DC2390_full_datapath_test_oldclient.py" script.  As you can see, there are frequent "TIMED OUT!!" messages.

    Python 2.7.16 |Anaconda, Inc.| (default, Mar 14 2019, 15:42:17) [MSC v.1500 64 bit (AMD64)]
    Type "copyright", "credits" or "license" for more information.
    
    IPython 5.8.0 -- An enhanced Interactive Python.
    ?         -> Introduction and overview of IPython's features.
    %quickref -> Quick reference.
    help      -> Python's own help system.
    object?   -> Details about 'object', use 'object??' for extra details.
    
    runfile('D:/Program_Files/Analog Devices/linear_lab_tools64/python/llt/app_examples/ltc2500_family/DC2390_full_datapath_test_oldclient.py', args='192.168.1.6', wdir='D:/Program_Files/Analog Devices/linear_lab_tools64/python/llt/app_examples/ltc2500_family')
    Tuning Word:131072
    Starting client
    FPGA load type ID: 0001 - Expecting ABCD, make sure you know what you're doing!
    FPGA load revision: 0103 - Minimum is 1246, make sure you know what you're doing!
    Setting up system parameters.
    
    Okay, now lets blink some lights and run some tests!!
    Software immediate trigger...
    ready signal is 4
    After 0.0019998550415 Seconds...
    Starting address: 
    6924160
    Reading a block of less than 1M points
    Standard Deviation: 0.0
    D:/Program_Files/Analog Devices/linear_lab_tools64/python/llt/app_examples/ltc2500_family/DC2390_full_datapath_test_oldclient.py:172: RuntimeWarning: divide by zero encountered in log10
      fftdb = 20*np.log10(fftdata / 2.0**31)
    RMS voltage: 0.0
    Peak-to-Peak voltage: 0.0
    Software immediate trigger...
    ready signal is 0
    After 0.105000019073 Seconds...
    TIMED OUT!!
    Starting address: 
    7603828
    Reading a block of less than 1M points
    Software immediate trigger...
    D:/Program_Files/Analog Devices/linear_lab_tools64/python/llt/app_examples/ltc2500_family/DC2390_full_datapath_test_oldclient.py:197: RuntimeWarning: divide by zero encountered in log10
      fftdb = 20*np.log10(fftdata / 2.0**31)
    ready signal is 0
    After 0.103999853134 Seconds...
    TIMED OUT!!
    Starting address: 
    8284380
    Reading a block of less than 1M points
    Software immediate trigger...
    D:/Program_Files/Analog Devices/linear_lab_tools64/python/llt/app_examples/ltc2500_family/DC2390_full_datapath_test_oldclient.py:210: RuntimeWarning: divide by zero encountered in log10
      fftdb = 20*np.log10(fftdata / 2.0**31)
    ready signal is 0
    After 0.105000019073 Seconds...
    TIMED OUT!!
    Starting address: 
    8965876
    Reading a block of less than 1M points
    Software immediate trigger...
    ready signal is 4
    After 0.00200009346008 Seconds...
    TIMED OUT!!
    Starting address: 
    15889536
    Reading a block of less than 1M points
    Software immediate trigger...
    ready signal is 4
    After 0.0019998550415 Seconds...
    TIMED OUT!!
    Starting address: 
    22813972
    Reading a block of less than 1M points
    
    
    
    
    
    
    
    
    
    
    Writing downward ramp to LUT!
    1073741835
    Done writing to LUT! Hope it went okay!
    Test done! Enter "client.shutdown()" to shut down SoCkit board.

  • The output says that you have the wrong FPGA load type and load revision.

    Did you follow the attached instructions when writing the SD card?

    https://rocketboards.org/foswiki/view/Documentation/ArrowSoCKITEvaluationBoardLinuxGettingStarted

  • Yes - I precisely followed the instructions for writing the SD card and used the image that you linked (above) in your first response to my posting.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.