Hi
I have two questions about AD7616.
Would you tell me the answer about these?
Question 1
Is there any problem if sequence is to power up VCC slightly first , followed by VDRIVE?
Question 2
Regarding to absolute maximum ratings of VDRIVE to AGND.
This rating is -0.3V to VCC + 0.3V, but recommended sequence is to power up VDRIVE first , followed by VCC.
Would you please explain these contents?
Best Regards,
Hi,
The AD7616 is robust to power sequence. But I would recommend following the one indicated in the abs/max rating.
Regards,
Jonathan
Hi ,
Do you have an update with regards to this issue?
If we follow the abs/max rating then we have to change the power-up sequence.
If So will the datasheet be changed in the future?
Thanking you
With best regards
Could you please update on this issue.
with best regards and wishes