In the spec for the AD2S1210 it lists a min voltage for the logic outputs of 2.4V when Vdrive is between 2.7V and 5.25V. Does this mean that if I power Vdrive with 5V I could get as low as 2.4V signals out? I would assume the 2.4V spec is for 2.7V on Vdrive, but I can't find any data for if it's higher than 2.7V. Is there a spec for min voltage at 5V?
In the spec for the AD2S1210 it lists a min voltage for the logic outputs of 2.4V when Vdrive is between 2.7V and 5.25V. Does this mean that if I power Vdrive with 5V I could get as low as 2.4V signals…