Post Go back to editing

AD7293 Eval board

Hello All,

I am facing a problem regarding writing a value to a certain register in AD7293 evaluation board.

In the configuration page (0x02), for the address 0x23 which is the register regarding background monitoring of some certain values, as much as try I cannnot enable background conversions for RSx+mon values which are bits D8-D11.

I write 1 to the corresponding bits (1111) but when I re-read this very register only the bit associated to RS3+mon is enables and the rest get disable again! (1111 turn to 1000).

and I tried by different combination of  values intending to enable some RSx+ pin and each time also the reserved value (bit D12-D15) changes from 0 to different values, and again bits related to RSx+ turn to 0.

I also tried to figure out if it is a protection mechanism and some other registers need to be configured before enabling the RSx+, but throughout datasheet I couldn't find anything.

I would appreciate if someone can help me.

Thanks in advance.

Regards,

Sara

Edit Notes

tag
[edited by: lallison at 5:07 PM (GMT 0) on 16 Jul 2019]

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.