Post Go back to editing

AD7293 Eval board

Hello All,

I am facing a problem regarding writing a value to a certain register in AD7293 evaluation board.

In the configuration page (0x02), for the address 0x23 which is the register regarding background monitoring of some certain values, as much as try I cannnot enable background conversions for RSx+mon values which are bits D8-D11.

I write 1 to the corresponding bits (1111) but when I re-read this very register only the bit associated to RS3+mon is enables and the rest get disable again! (1111 turn to 1000).

and I tried by different combination of  values intending to enable some RSx+ pin and each time also the reserved value (bit D12-D15) changes from 0 to different values, and again bits related to RSx+ turn to 0.

I also tried to figure out if it is a protection mechanism and some other registers need to be configured before enabling the RSx+, but throughout datasheet I couldn't find anything.

I would appreciate if someone can help me.

Thanks in advance.

Regards,

Sara

Edit Notes

tag
[edited by: lallison at 5:07 PM (GMT 0) on 16 Jul 2019]
Parents
  • Hi Sara,

    Unfortunately the readback from this register is slightly different than other registers.

     

    While writing to this register the data format is as follows.

    Bit

    D15 – D12

    D11 – D8

    D7 – D4

    D3 – D0

    Function

    Reserved

    RS3+MON – RS0+MON

    BI-VOUT3mon – BI-VOUT0mon

    VDD3 – VDD0

    However when reading from this register, the data format is:

    Bit

    D15

    D14 – D11

    D10 – D8

    D7 – D4

    D3 – D0

    Function

    Reserved

    RS3+MON – RS0+MON

    000

    BI-VOUT3mon – BI-VOUT0mon

    VDD3 – VDD0

    The data (i.e. the RSx+MON background enable status) in the upper byte is shifted.

    Regards,

    Valerie

Reply
  • Hi Sara,

    Unfortunately the readback from this register is slightly different than other registers.

     

    While writing to this register the data format is as follows.

    Bit

    D15 – D12

    D11 – D8

    D7 – D4

    D3 – D0

    Function

    Reserved

    RS3+MON – RS0+MON

    BI-VOUT3mon – BI-VOUT0mon

    VDD3 – VDD0

    However when reading from this register, the data format is:

    Bit

    D15

    D14 – D11

    D10 – D8

    D7 – D4

    D3 – D0

    Function

    Reserved

    RS3+MON – RS0+MON

    000

    BI-VOUT3mon – BI-VOUT0mon

    VDD3 – VDD0

    The data (i.e. the RSx+MON background enable status) in the upper byte is shifted.

    Regards,

    Valerie

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.