Post Go back to editing

FAQ: How to calibrate the gain error introduced by a resistor on the AD7606B's front end?

I have a series resistor in front of my analog inputs that causes a gain error, how can I calibrate this gain error off with AD7606B?

  • Having a series resistor in front of the ADC leads to having a system gain error. This system gain could be calibrated on the backend, however the AD7606B provides a feature to compensate this error by just programming the resistor value used on the front-end (up to 65kOhm). This gain calibration register reduces the burden of doing this task on the backend, and achieves it more precisely because the it uses the actual, factory trimmed, input impedance on each device. See A.N. 2011 for further details on AD7606B gain calibration feature, and simulate it through the Software model available on the AD7606B product page