LTC2439-1

Hi!

We wanna use the LTC2439-1 configured with 16-Channel Single-Ended Inputs, the Reference-Voltage is 5.0V and the Input-Channel Voltages are from 0-5.0V

But the datasheet does not clearly describe the function for us with this configuration.

We are not sure if the LTC2439-1 converts a Input-Channel Voltage from 0-5V (CHx/COM) to a 16-Bit result (with the above decribed configuration) ?

Or the channel voltage must be between -FS (-0.5 * Vref) and +FS (0,5 * Vref) ?

Thank you !

Martin

Parents Reply Children