KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
October Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Finding Your Circuit Chi — EMC Quiz!
Think you know EMC? Test your knowledge with our 5-question quiz!
Read the blog first, then take the challenge: Finding Your Circuit Chi
Every current flowing creates electromagnetic fields.
Strong EMC design
View All
AD7797
Production
The AD7796/AD7797 are complete, analog front ends for high
precision, bridge sensor applications such as weigh scales. The
AD7796/AD7797 contain a Σ-âˆ...
Datasheet
AD7797 on Analog.com
Hi everyone,
I am working on AD7797, created a custom PCB with atmega328p chip(arduino uno) and also written firmware for this. I am able to communicate with AD7797 but while reading ADC value it false data. Same data repeats. Please help me i am attaching PCB schematic and arduino code. Kindly share some library or code for AD7797.
Regards
Suman
#include <SPI.h> // include the SPI library:
#define cs 10
void setup()
{
Serial.begin(9600); // initialize serial port
pinMode(SCK, OUTPUT);
pinMode(MOSI, OUTPUT);
pinMode(MISO, INPUT);
pinMode(cs, OUTPUT);
digitalWrite(cs, HIGH);
SPI.begin(); // wake up the SPI
SPI.setDataMode(SPI_MODE3); // datasheet p6-7
SPI.setBitOrder(MSBFIRST);
SPI.setClockDivider(SPI_CLOCK_DIV32); // datasheet p6
Serial.println("AD7797 Test");
initAD7797();
}
void initAD7797()
{
beginAD7797();
resetAD7797(); //reset device
delay(2);
if (!(getID() % 2))
{
Serial.println("ID : AD7796");
}
else
{
Serial.println("ID : AD7797");
}
Serial.print("Configuration : "); Serial.println(readCFG(), BIN);
}
void beginAD7797() //must be mode3
{
//SPCR = (1<<SPE)|(1<<MSTR)|(1<<CPOL)|(1<<CPHA)|(1<<SPR0); //mode3, 1MHz
SPCR = (1 << SPE) | (1 << MSTR) | (1 << CPOL) | (1 << CPHA); //mode3, 4MHz
}
void resetAD7797() //p14
{
digitalWrite(cs, LOW); //reset IC by sending out 32b of 1s
transferAD7797(0xFF);
transferAD7797(0xFF);
transferAD7797(0xFF);
transferAD7797(0xFF);
digitalWrite(cs, HIGH);
}
uint8_t getID() //WORKS!
{
uint8_t output = 0;
digitalWrite(cs, LOW);
transferAD7797(0x60); //01100000 0x60
output = transferAD7797(0x00);
digitalWrite(cs, HIGH);
return output;
}
//read value from ADC,
long readAD7797()
{
long value = 0; //uint16_t byte1, byte2, byte3;
//selectCH(ch);
selectMode();
while (readST() > 127); //wait until !RDY
digitalWrite(cs, LOW);
transferAD7797(0x58); //select DATA register (01011000)(0x58) //one read try (01011100)(0x5C) for CREAD
value = (transferAD7797(0x00) << 16) & 0xFF0000;
value += (transferAD7797(0x00) << 8) & 0xFF00; //grab top byte
value += transferAD7797(0x00) & 0xFF; //grab bottom byte
digitalWrite(cs, HIGH); //pull CS high to disengage
return value; //return( ((byte1<<8) | byte2) & 0xFFFF);
}
uint16_t readCFG() //works!
{
long output = 0;
digitalWrite(cs, LOW);
transferAD7797(0x50); //select CONFIGURATION register (01010000)(0x50)
output = (transferAD7797(0x00) << 8) & 0xFF00; //grab top byte
output += transferAD7797(0x00) & 0xFF; //grab bottom byte
digitalWrite(cs, HIGH);
return output;
}
uint8_t readST() //works!
{
long output = 0;
digitalWrite(cs, LOW);
transferAD7797(0x40); //select STATUS register (01000000)(0x40)
output = transferAD7797(0x00); //grab byte
digitalWrite(cs, HIGH);
return output;
}
//select adc channel
void selectCH(uint8_t ch)
{
if (ch > 2)
ch = 2;
ch |= 0x90;
digitalWrite(cs, LOW); //pull CS low to engage
transferAD7797(0x10); //select configuration register 00010000 (0x10)
transferAD7797(0x10); //Write 16 bits to CONFIGURATION register:
//bias voltage: disabled 0 0
//burnout current: disabled 0
//bipolar operation: 0 or 1?
//boost: disabled 1
//gain: disabled 0 0 0
//top 8b: 00011000 (0x18), disable boost yields 00010000 (0x10)
transferAD7797(ch); //internal reference 1
//0 0
//buffer 1
//0
//000 (CH1) 001(CH2) 010(CH3)
//channel select = AIN1(+) - AIN1(-)
//bottom 8b: 10010000 (0x90) 10010001 (0x91) read CH2 10010010 (0x92) read CH3
digitalWrite(cs, HIGH); //pull CS high to disengage
}
void selectMode()
{
digitalWrite(cs, LOW); //pull CS low to engage
transferAD7797(0x08); //select MODE register (00001000)(0x08)
//Write 16 bits to MODE register on page 16 Table 15
transferAD7797(0x20); //0x00 for continuous
//0x20 for single conversion preferred
//0x40 for idle
//0x60 for power down
//0x80 internal zero scale calibration
//0xA0 internal full scale calibration
//0xC0 system zero scale calibration
//0xE0 system full scale calibration
//update rate on page 16/17
transferAD7797(0x0C); //0x00 X X
//0x01 470Hz 4mS
//0x02 242Hz 8mS
//0x03 123Hz 16mS
//0x04 62Hz 32mS
//0x05 50Hz 40mS
//0x06 39Hz 48mS
//0x07 33.2Hz 60mS
//0x08 19.6Hz 101mS -90dB for 60Hz
//0x09 16.7Hz 120mS -80dB for 50Hz
//0x0A 16.7Hz 120mS -65dB for 50/60Hz
//0x0B 12.5Hz 160mS -66dB for 50/60Hz
//0x0C 10Hz 200mS -69dB for 50/60Hz
//0x0D 8.33Hz 240mS -70dB for 50/60Hz
//0x0E 6.25Hz 320mS -72dB for 50/60Hz
//0x0F 4.17Hz 480mS -74dB for 50/60Hz
digitalWrite(cs, HIGH);
}
uint8_t transferAD7797(uint8_t data)
{
beginAD7797(); //set correct SPI settings for devices
SPDR = data;
while (!(SPSR & (1 << SPIF))); //wait until transfer is done
return SPDR; //return received byte
}
void loop()
{
delay(100);
Serial.println(String("ADC Read : ") + readAD7797());
}
Kindly help anyone
Hi,
Do you have a scope shot of your digital interface upon reading the data register? Are you also monitoring the RDY bit or RDY pin upon reading the data register? May I know also what is your input range and so what data output are you getting from these input values?
We have a software driver for the AD779x family. This can be also applicable for the AD7797. So you can use this as your reference code. Hope this will help. Kindly refer to the link. AD7793 IIO Low Power Sigma-Delta ADC Linux Driver [Analog Devices Wiki]
Thanks,
Jellenie
Hi thanks for the response. I read your solution on other related post accordingly i am trying, kindly can you check the above attached code. Also the reference code which you shared is bit complex and i am not expert in programming. If you tell me simple way it will be great help. Also please explain the sequence of data read write.
I followed figure 17 of datasheet (page 23) AD7797 for making PCB. I just want a simplest way to read ADC 24 bit value. Please provide some sample code written in C or C++ or Arduino
Please reply
Hi,
Apologies. I have attached the wrong link. You can use this link of AD779x generic driver for any microcontroller
https://wiki.analog.com/resources/tools-software/uc-drivers/renesas/ad7793
We do not usually provide support in terms of software, we only provide code to control and initialize the AD779x part but we don't provide any actual details for a specific communication protocol to the ADI driver but if you have any other issue regarding the driver provided on the link above you may ask directly to the Microcontroller no-OS Drivers community to support you.
Thanks,
Jellenie
Hi Jellenie
I tried everything but not getting the to read properly. Accordiing to your advice i wrote again a simple program. I can see data in and out on DSO, but not able to decode to meaningful data. Kindly help.
here i am attaching DSO snapshots and new code please once you check it the sequence.
Regards
Suman


#include <SPI.h> // include the SPI library:
char csPin = 10; //where chipselect pin connected
//===================================================================================
void setup()
{
Serial.begin(9600);
// spi setup
SPI.begin(); // wake up the SPI
SPI.setDataMode(SPI_MODE3); // datasheet p6-7
SPI.setBitOrder(MSBFIRST);
SPI.setClockDivider(SPI_CLOCK_DIV32); // datasheet p6
delay(100);
Serial.println("AD7797 Test");
Serial.println("Reseting...");
delay(2000);
// adc setup
adc_reset();
Serial.println("Reset Done");
if (!(getID() % 2))
{
Serial.println("ID : AD7796");
}
else
{
Serial.println("ID : AD7797");
}
adc_config();
Serial.print("Ready");
Serial.print("\n\n");
}
//===================================================================================
void loop()
{
Serial.println("Waiting...");
adc_config();
Serial.println(String("Raw Data : ") + (adc_read(), BIN));
delay(5000);
}
//===================================================================================
void adc_reset() {
unsigned char incomingByte = 0;
digitalWrite(csPin, LOW);
for (int i = 0; i < 4; i++) { // send 0xFFFFFFFF
incomingByte = SPI.transfer(0xFF);
}
digitalWrite(csPin, HIGH);
delayMicroseconds(500); // (datasheet --> p.23 ~p.19) wait 500us
}
//===================================================================================
uint8_t getID() //WORKS!
{
uint8_t output = 0;
digitalWrite(csPin, LOW);
SPI.transfer(0x60); //01100000 0x60
output = SPI.transfer(0x00);
digitalWrite(csPin, HIGH);
return output;
}
//===================================================================================
uint8_t readST() //works!
{
long output = 0;
digitalWrite(csPin, LOW);
SPI.transfer(0x40); //select STATUS register (01000000)(0x40)
output = SPI.transfer(0x00); //grab byte
digitalWrite(csPin, HIGH);
return output;
}
//===================================================================================
// read from data register
uint32_t adc_read()
{
uint32_t registerValue = 0;
byte incomingByte;
while (readST() > 127); //wait until !RDY
digitalWrite(csPin, LOW);
SPI.transfer(0x58); // read from data register
for (int i = 0; i < 3; i++) {
incomingByte = SPI.transfer(0x00);
switch ( i ) {
case 0:
registerValue = incomingByte;
break;
case 1:
registerValue <<= 8;
registerValue |= incomingByte;
break;
case 2:
registerValue <<= 8;
registerValue |= incomingByte;
break;
}
}
digitalWrite(csPin, HIGH);
return registerValue;
}
//===================================================================================
void adc_config()
{
adc_cr_write(0x17, 0x10); // unipolar, channel 0
adc_mode_write(0x20, 0x0c); //10Hz 200mS -69dB for 50/60Hz
}
//===================================================================================
void adc_cr_write(char FirstByte, char SecondByte) {
unsigned char incomingByte = 0;
digitalWrite(csPin, LOW);
incomingByte = SPI.transfer(0x10); // write in config register
incomingByte = SPI.transfer(FirstByte); // data for write
incomingByte = SPI.transfer(SecondByte); // data for write
digitalWrite(csPin, HIGH);
}
//===================================================================================
void adc_mode_write(char FirstByte, char SecondByte) {
unsigned char incomingByte = 0;
digitalWrite(csPin, LOW);
incomingByte = SPI.transfer(0x08); //write in mode register
incomingByte = SPI.transfer(FirstByte); // data for write
incomingByte = SPI.transfer(SecondByte); // data for write
digitalWrite(csPin, HIGH);
}
//===================================================================================Hi Jellenie,
I have written mode and config register as (mode = 0x200C and config = 0x1710) which you can see on the attached snapshot serial window. I tried reading mode and config register, it is exactly what i set.
but now also when i am reading data resister the raw reading is max value like saturated.
please check image and let me know what is the correct sequence of reading
Finally something good, able to read adc 24 bit data. Thank you
Now need to calibrate. Can you tell how i can do this.
Regards
Suman
Hi,
Good to hear that you are now able to read the data. Regarding the calibration, We have an AD779xFAQ document that covers all of the information needed for calibrations. This may help you on your queries. Usually, an internal calibrations is performed first followed by system calibrations. If the errors after performing internal calibrations does not change or has minimal effect then that's the time you can consider performing a system calibration to remove the errors internal to ADC as well as the errors associated in your analog front end circuitry. For internal calibrations, the respective zero input and full-scale input are automatically connected internally to the ADC input pins. A system calibration, however, expects the system zero-scale and system full-scale voltages to be applied to the ADC pins before the calibration mode is initiated. In this way, external ADC errors are removed.
Thanks,
Jellenie
Thanks i will go through the document.
Can you check my pcb schematic is it correct? i followed datasheet for making.
Both +Vref and AVDD are at 5V analog
And -Vref abd AGND are analog ground.
I am not understanding datasheet for calibrating zero scale or full system, what physical connection do i need to make with AN+ and AN- while calibrating different calibration steps.
Please can you explain in details
Regards
Suman
Thanks i will go through the document.
Can you check my pcb schematic is it correct? i followed datasheet for making.
Both +Vref and AVDD are at 5V analog
And -Vref abd AGND are analog ground.
I am not understanding datasheet for calibrating zero scale or full system, what physical connection do i need to make with AN+ and AN- while calibrating different calibration steps.
Please can you explain in details
Regards
Suman
Hi, Suman.
I cannot see clearly the attached schematic. Do you have a PDF file? Regarding the same source for VREF and Analog supply, it's okay as long as you can ensure that the source is stable and not noisy. For internal calibration, you do not need to connect anything as the zero and full scale input are automatically connected internally to the ADC input pins. For system calibrations, system zero-scale and system full-scale voltages need to be applied to the differential ADC pins (AIN+ and AIN-) before the calibration mode is initiated.
Thanks,
Jellenie
Please check below link to access schematic pdf. PDF upload is not given here. For system calibration full scale 5V i need to apply across AIN+ and AIN- am i correct? Please explain in detail
Regards
Suman
Waiting for the reply
Please reply anyone i am waiting. Is this the support you give, partial.
Hi,
Yes, for system full scale calibration, you have to apply your full scale or maximum input voltage across AIN+ and AIN- (in your case in a load cell application it's the Max load that your sensor can measure, and in system zero scale you have to apply the smallest input voltage across AIN+ and AIN-, (that is no load at all).
Thanks,
Jellenie
Hi,
I had done good progress things are going good now.
One major issue i am facing now, that while reading channel AIN+ and AIN- my ADC output does not go more than 16777215 even if the differential voltage is increasing. It starts from 0 and goes max to 16777215 and after that no change exact same ADC value it gives.
Is it because of calibration, or what i should do. Please reply soon.
Regards Suman
Sorry i understood, 16777215 is the 24 bit max value. But this max value i am getting at 39mV only according to datasheet (P20) its correct for 5V +Vref. I want to understand how i can sense differential voltage of range 1V to 1.8V. In my application voltage across AIN+ and AIN- is in range of (1.5V to 1.85V)
Please help me how to solve this
Regards Suman
Hi,
AD7797 has a fixed gain=128, thus your differential inputs is limited to +/-Vref/128 = +/-39 mV. May I know what is the specifications of your load cell (i.e. sensitivity, max. load, etc.). If you want to measure a differential voltage of 1.5V to 1.85V then you have to add an analog front end that will attenuate your input signal to meet the AD7797 input specification. Another option is to use other parts that can accept your required inputs without the need of external circuitry such as AD719x or AD7124 which has lower noise and lower current consumption than the AD7797 with some advanced features. AD7124 operates from a 3.6V max supply but is worth considering 3V supply is acceptable in your design.
Thanks,
Jellenie
Load cell is nothing but custom designed strain guage wheatstone bridge. And i don't have much detail about it. Just i measured at 5V excitation voltage it takes 10 mA current, and it generates differential voltage 1.65V which i want to measure with to measure.
At this point i can't go to any other chip. Already more than a month gone in getting pcb, components and all.
Kindly help me this chip only.
What circuity is required to make it work
Hi,
Since your input is outside the required specifications of AD7797, you have to attenuate your signal either using a voltage divider or an amplifier with gain= -8 that could lower your 1.65V to 20mV.
Thanks,
Jellenie