Dear EZ community,
I've ordered the 2289A-B and DC590 boards to read out the LTC2368-24 ADC with PYTHON.
To read out the LTC2368, there are code snippets for the 16bit and 18bit version with the DC890 board.
My question: can I simply adapt the code snippets from LinearLabTools in the llt/common folder in terms of duplicating the dc890.py" and creating a dc590.py file? I've seen functions for the dc590 already in the ltc_controller_comm.py-file
Also, I’m unsure about the clock, because it says an external clock is not needed if a QuikEval controller is used.
Could you help me out with some hints about setting a clock frequency for the DC2289-board? Also the data readout from the ADC, can I simply duplicate a file in the llt\demo_board_examples\ltc23xx\ltc2368-directory and rename the according board types (e.g. 780 to 590 and 1796 to 2289)?
Best regards,
Robert
typo corrected
[edited by: RobertS at 3:59 PM (GMT -5) on 21 Nov 2018]