Post Go back to editing

LTC2324 tCYC Time between Conversions Max time

Thread Summary

The user inquires about the impact of variable time between conversions (tCYC) on ADC accuracy for the LTC2324-12 and similar ADCs (LTC2325, LTC2320, LTC2351, LTC2357). The final answer confirms that exceeding the maximum tCYC of 1000us can lead to a gradual loss of accuracy. For variable repetition rates in a DPSS laser application, the user must either add conversions during idle times or set the ADC into power-saving mode to maintain accuracy.
AI Generated Content

Q:

LTC2324-12 Datasheet Page 5 Line:

tCYC    Time between Conversions            (Note 11)  tCYC = tCNVH + tCONV + tREADOUT   min 0.5us  max 1000us

and Page 6  Note 11:

Note 11: Guaranteed by design, not subject to test.

----------------------------------------------------------------------------------------------------------------------

So, the minimum Sampling Frequency is 1/1000us = 1KSPS ? If Time between Conversions  is more than 1000us, the adc accuracy will be lost , or something is going wrong?

For application with variable tCYC, for example,  if tcyc sequence  like this : 1s 0.5s 100ms 10us  10s 1us 2ms 1us 1us 1us 5s........  , does the adc results will be right?

Thanks.

Does this can be applied for LTC2325 LTC2320 LTC2351  LTC2357 ...series?

Thanks.

Parents
  • If the time between conversions exceeds the maximum specified, there will be a gradual loss of accuracy.  This also applies to parts such as the LTC2325, etc.  Let me know if you have a specific concern or time between conversions and I can help you further.

  • I see.

    This is the Application:

    DPSS ( Diode-pumped solid-state laser ). Repetition rates :0Hz to 100 kHz. 

    The adc is used to monitor the peak current of  pulsed pumped diodes for DPSS test in its production. Repetition rate is variable, so the time between conversions is variable. When one pulse is detected, the adc works at 2Msps for several samples, then the sample values can be averaged. When one pulse is gone , there will be a long time before next pulse, maybe 10us to several seconds depending on the repetition rate, so i have a concern on time between conversions.

    As a result, If I use this serial adcs, I must add conversions in the long idle time or set the adc into power saving mode.

Reply
  • I see.

    This is the Application:

    DPSS ( Diode-pumped solid-state laser ). Repetition rates :0Hz to 100 kHz. 

    The adc is used to monitor the peak current of  pulsed pumped diodes for DPSS test in its production. Repetition rate is variable, so the time between conversions is variable. When one pulse is detected, the adc works at 2Msps for several samples, then the sample values can be averaged. When one pulse is gone , there will be a long time before next pulse, maybe 10us to several seconds depending on the repetition rate, so i have a concern on time between conversions.

    As a result, If I use this serial adcs, I must add conversions in the long idle time or set the adc into power saving mode.

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.