Hello,
I have a EVAL- AD2S1210SDZ with a EVAL-SDP-CB1Z board and want to Run the AD2S1210SDZ in standalone mode.
The board is needed to convert resolver signals to encoder signals at 12 bit (4096).
I Need help with the configuration Jumper pins. When i have RES0 and RES1 in position C and LK4 and LK5 in Position C, After configuring using the board i can read the data and Get 4096 count with a sin/ cos clipped error.
So my questions are:
- How do i get the same resolution in the standalone mode. i have tried using the jumper locations in the datasheet and have failed.
i have attached an image of the current set up of the board.
Any help on this is much appreciated.