Hi,
I want to use AD2S1210 for Resolver which has excitation voltage of 7Vrms and 10KHz frequency.
Resolver Excitation Voltage : 7Vrms
Resolver Output Voltage : 2V
Can I use AD2S1210 directly of some gain factors are required?
AD2S1210
Production
The AD2S1210 is a complete 10-bit to 16-bit resolution tracking resolver-to-digital converter, integrating an on-board programmable sinusoidal oscillator...
Datasheet
AD2S1210 on Analog.com
Hi,
I want to use AD2S1210 for Resolver which has excitation voltage of 7Vrms and 10KHz frequency.
Resolver Excitation Voltage : 7Vrms
Resolver Output Voltage : 2V
Can I use AD2S1210 directly of some gain factors are required?
Pankaj,
You will require voltage amplification on the EXC/EXCb pair to achieve the required 7VRMS excitation voltage. I would also recommend that you verify the transformation ratio to ensure that the resolver output magnitude will also be within the range of the input otherwise you may observe loss of signal faults.
Sean