Request for Support to Analog Input & Output Isolation Circuit From/ to ADC & DAC

Hello Sir/ Mam,


 We are Using 4-Channel ADC & 8-Channel DAC in one of our project.

This project mainly used for industrial control application.



8-Channel DAC specification

· Each channel Maximum ±10V analog outputs
· 16-bit resolution
· Simultaneous channel update



4-Channel ADC specification

- Each channel Maximum input Voltage 0-32V
· 24-bit resolution

CPU controls ADC & DAC.

How to isolate Analog inputs & outputs?

where should be the isolation circuit placed ( whether before or after the ADC/ DAC ) ?
Please recommend us relevant Isolation circuit part.


Regards

Lakshmanan V