1. Top of page 73 is quoted below, but Figure 109 itself on previous page shows the connections swapped (DOUT0 and DOUT1 to DOUT7 and DOUT6, respectively). Which version (text or figure) is the correct one? Which data input pin should be used when AD7768 (8-channel version) is daisy-chained with DOUT0 only: DOUT6 or DOUT7?
2. The datasheet now documents that the FILTER pin should be logic 1 for use with a crystal. Previous discussion in this forum shows it should be 0 for use with LVDS clock, but that is not mentioned in the datasheet.
Edit Notes
typo[edited by: marekm at 11:01 AM (GMT -4) on 27 Sep 2018]