Article AD7745: Capacitance Application

1.:What is the difference between the AD7745 and the AD7747? Is it only the
different resolution and accuracy and the input range?
2.:What is the difference between the models for the AD7746: ARUZ / REEL / REEL
7 ?
3.:If the resolution of the AD7746 is stated as down to 4aF, can I really
measure a change in capacity of 4aF with it?
4.:Is it possible to measure capacities much larger than the specified maximum
CAPDAC range of +13pF...+21pF for the AD7746? I read something of lowering the
excitation voltage or using another capacity in series. Does that effect the
resolution/accuracy much?
5.:If I want to use an evalution board, is it really that simple, that I only
connect my capacity to the CDC and the CDC to the eval-board and that to the PC
via USB? And then I get the capacity shown in the evaluation software?

 

1 The major change of the Ad7747 is the Input range of 8pF ( as opposed to 4pF
for the ad7745) The power consumption is also slightly less.

2 the ARUZ is a single device whereas the REEL is a standard reel of
devices(2500 devices). The REEL7 is a smaller REEL width again.

3  Yes , 4pF is full scale, 4fFis Absolue Error - your mail is showing aF.

4 See application information in the datasheet for this information. But this
is possible.

5 I can recommend the evaluation PCB, but this has its own sensor, where you
slide a dielectric between plates. But you should be able to connect to the
Eval PCB, once your Capacitor is in this region of operation.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.