Article AD7960 LVDS test pattern

Question

Could you forward me LVDS test patterns for AD7960 ADC, I cannot find them in
the data sheet.

Answer

The AD7960 generates an 18-bit pseudo random test pattern based on the
polynomial series - . To generate this pattern, you need to power-up the AD7960
and set EN[3:0] = 0100. Then Initiate a conversion CNV± and run the CLK± at
200MHz (max up to 300MHz). The pseudo random generator is reset into a known
state at the start of the first conversion. At the end of conversion, the
pseudo random number is loaded into the LVDS block instead of the 18-bit
conversion result. The pseudo random number can be read back the same way the
conversion result is read back. To exit this mode, you need to change EN[3:0]
from 0100 to any other combination mentioned in the datasheet.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.