Article The AD4114 datasheet specifies that AVDD must be 5V, in the section on Single-Supply Operation. However, can AVDD can also be 3.3V when AVSS is 0V?

Answer:

This appears to be an error in the AD4114 datasheet and should be corrected in a future revision.

The AVDD supply can be either 3.3 V or 5 V.

AVDD - AVSS can go from 3V to 5.5V as specified in the table below. 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.