Article Q2. On the AD4111/AD4112/AD4114/AD4115 can I detect if the input signals are floating due to faulty wiring?

Q2. On the AD4111/AD4112/AD4114/AD4115 can I detect if the input signals are floating due to faulty wiring?

AD4111 provides a unique solution for open wire detection on the voltage inputs from a single 5V/3.3V supply. Open wire detection is calculated by comparing the difference between the two-channel conversions to a certain threshold. Details can be found on page 27 in the Open Wire Detection section of the AD4111 datasheet.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.