Q: What is the correct power supply sequence for the ADAS3023 to operate properly?
A: The ADAS3023 requires these five supplies: AVDD = +5V, DVDD = + 5V, VDDH = + 15V, VSSH = - 15V, and VIO = 1.8V…
Q
What is the headroom requirement of the ADAS3023 inputs from the high voltage supplies?
A
In other words, the specified operating input voltage of any input pin requires at least 2.5 V of headroom…
Q
What are the recommended ADC driver, external reference and reference buffer options?
A
The ADAS3023 datasheet recommends the ADA4841 and AD8031 as ADC driver (to drive auxiliary input pair …
Q
What are the target markets/applications for this product?
A
The ADAS3023 is highly integrated, leading to significantly reduced signal chain form factor, and competitively priced making it ideal…
Q
What package is this part offered in?
A
The ADAS3023 is offered in a 6mm X 6mm, 40 lead, Lead Frame Chip Scale Package (LFCSP_VQ) with pin pitch of 0.5mm.
Question Is there an evaluation board for the ADAS3023? Answer Yes, the EVAL-ADAS3023EDZ board can be used to evaluate the ADAS3023 part,
which is compatible with the Converter Evaluation and Development…
Question Is there an IBIS model available for the ADAS3023 Answer Yes, please follow the link below:
http://www.analog.com/en/analog-to-digital-converters/ad-converters/adas3023/pro
ducts/product.html#product…
Question What types of input signals the ADAS3023 can support? Answer The ADAS3023 can resolve the single ended unipolar or bipolar inputs using any
of the four input ranges ±2.56 V, ±5.12 V, ±10.24…
Question What power supplies does the ADAS3023 require? Answer The ADAS3023 requires these five supplies: AVDD = +5V, DVDD = + 5V, VDDH = +
15V,
VSSH = - 15V, and VIO = 1.8V to 5V. The user must bring…
Question I developed my own measurement board based on the ADAS3023. I am having issues
with the ADAS3023, sometimes after a RESET or Power On the part is not
functioning as expected. Answer Check…