Q: I am able to read raw data for my leads/electrodes, how do I convert this raw data to an ECG voltage?
Firstly decide the operating mode. Here are 3 main operating modes on the ADAS1000: Analog Lead…
The ADAS1000 contains different modes of operation, deciding which to use can be a bit confusing, here's a little guidance and also some example calculations in attached excel sheet (see below)
Analog…
Purpose : The ACLO block within the ADAS1000 is used to help user identify if an electrode has fallen off or if the connection is poor (higher impedance). This document captures some detail around the…
The ADAS1000 has a very flexible digital pace detection algorithm with a lot of programmability for various thresholds used in the pace detect algorithm. Please consult this in conjunction with the ADAS1000…
Q: I'm evaluating the ADAS1000 and I don't have a patient simulator, how else might I evaluate the device? can I use a signal/function generator
A: As the EVAL-ADAS1000SDZ was designed for evaluation…
The ADAS1000 oscillator circuit requires total capacitance seen at the XTAL pins <20pF (ideally <15pF) to ensure reliable start up across operating conditions.
For some crystal oscillators, the pad footprint…
The purpose of this document is to describe a little more about the DRDYb operation of the ADAS1000. This should be read in conjunction with the ADAS1000 datasheet descriptions.
There are two modes of…
Q : I want to use your ADAS1000 in my ECG application and I need software drivers/starting point/sample code for interfacing to my ucontroller/DSP/ linux environment
A : On our WIKI webpage, we have…
Traditionally ECG applications have tended to be AC coupled systems, more recently DC coupled approaches are becoming more popular for various reasons. There are advantages and disadvantages to each approach…
Q : I've purchased an ADAS1000 evaluation board, the EVAL-ADAS1000SDZ and I need to know how to connect my patient simulator to the board?
A: As documented in the User Guide, UG-426 , the ADAS1000 evaluation…