AD7768: FAQ

  • Created
  • Updated
Was this helpful?
  • AD7768 FAQ - The input seems to be switching faster than the 256 kSPS rate?

    The analog input seems to be switching faster than the 256 kSPS output data rate, is this correct? This is a common question for sigma delta ADC architectures like the AD7768 (and the AD7768-4, AD7761…
  • AD7768 FAQ - What front end driver amplifier is suitable to drive the AD7768?

    There are many amplifiers suitable to drive the AD7768/AD7768-4. Choosing the most suitable amp can be a difficult task, especially when there are constraints on the system power. In order to achieve the…
  • AD7768 FAQ - What is a SYNC and when is it required?

    The SYNC command on the AD7768 can be thought of as a reset of the digital filter paths and logic within the AD7768. One of the major events that the sync triggers is the reloading of the digital filter…
  • AD7768 FAQ - What is the maximum input common-mode voltage?

    Some architectures of ADC require that the input common-mode voltage of the applied analog signal be within a certain specified range, which is often close to the midpoint of the analog input range. …
  • AD7768 SYNC vs. RESET

    The AD7768 is an 8-channel, simultaneous sampling Σ-Δ analog-to-digital converter (ADC) with a Σ-Δ modulator and digital filter per channel, enabling synchronized sampling of ac and dc signals. The AD7768…
  • AD7768/AD7768-4 FAQ - Clock Selection

    The AD7768/AD7768-4 MCLK can be applied by using one of the three different options that are available to the user. The purpose of this document is to further explain these three options and how they are…
  • AD7768: EVB Source Code

    Question: I want to test more function(and performance) with AD7768 EVB and need to modify its code, Does ADI can provide the AD7768 EVB Source Code and EVAL-SDP-CB1Z protocal to us? Thanks. I…
  • AD7768: What is the analog input range?

    The input voltage range of the ADC depends on the analog voltage supplies (AVDDx and AVSSx), the reference used (Vref), the configured PGA gain and the type of signal connected to the input (single ended…
  • EVAL-AD7768 Evaluation Board Quick Start Guide

    The EVAL-AD7768FMCZ evaluation kit features the AD7768, a 24-bit, 256 kSPS, analog-to-digital converter (ADC). This aim of this document is to create a quick start guide for the AD7768/AD7768-4 customer…
  • EVAL-AD7768FMCZ FAQ - How can I save sample data to a file?

    Data displayed on any of the graphs in the EVAL-AD7768FMCZ/ EVAL-AD7768-4FMCZ can be saved to a file for further processing. There is the option to export the data to the clipboard or to excel. This can…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.