Q
I want to connect several Capacitance to Digital Converters (AD7745, AD7746, AD7747) using the I2C bus. The question is how can I get the slave address of each device or how can set the slave address…
Q
1.:What is the difference between the AD7745 and the AD7747? Is it only the different resolution and accuracy and the input range? 2.:What is the difference between the models for the AD7746: ARUZ…
Q
Is it possible to extend the range of measured capacitances above 4 pF by decreasing excitation signal e.g. to a value of VDD/4 ?
A
1) Connect a known fixed capacitor in series with the sensor…
Q
The datasheet states that the max. common-mode cap for a AD7745 is 17pF. Is it possible to connect 50pF? Maybe with a voltage devider at EXCx?
A
1) Connect a known fixed capacitor in series with…
Q
They make humidiysensors with a capacitive output. Therefor, they have interests in CDC as AD7745. But the nominal capacitance of their sensors is 180pF with a max. change of +-50pF, which is higher…
Q
How to start a conversion in single conversion mode?
A
How to start a conversion in single conversion mode: It is the operation of writing "010" to the mode bits MD2-MD0 in the configuration…
Q
Are there some protection circuit in front of the AD7745 to limit the input voltage and current while not affecting the capacitance measurement.
A
the AD7745 has no over voltage protection please…
Q
What is the AD7745 long term drift behavior?
A
We guarantee accuracy within a 4fF band. In fact each part is factory tested to ensure that it is within a 2fF band; the extra 2fF then takes account…
Q
The absolute maximum ratings for AD7745 state the following; I expect this device to be able to tolerate the Pb free solder temperature of 260C , Is AD7745 able to withstand up to 260C during Pb free…