Article AD7738: Timing specs

Question

Please refer to Data Sheet Rev. 0 page 4. table: Timing Spec. What is the
meaning of t9: will the DOUT be tristated 10 to 80 ns after SCLK rising edge
sampling LSB, no matter if -CS is kept low? (t9 is referred to SCLK, not -CS)
Does it apply only to LSB, or DOUT is tristated t9 after each SCLK rising edge?
NEXT PROBLEM: t6+t7=100ns. Could I use 10MHz SCLK, and as t5=0..60ns, I can not
be sure of sampling by rising edge, so I would use falling edge?

Answer

Q1: The DOUT is an active logic output only during the read operation, i.e.,
during the time the data are being shifted out. For the rest, the DOUT is
tri-stated, regardless on CS. Therefore, the t9 is correctly related to the
last SCLK corresponding to the LSB in the read operation, i.e., to the 8th bit
when reading an 8-bit register, 16th bit when reading a 16-bit register, etc.

Q2: The t5 max of 60ns is specified with 50pF load on the digital output. The
load is usually less - and the max time should be shorter for lower capacitive
load. In my setup - AD7738 DOUT driving a standard ADuC824 digital input + 15pF
oscilloscope probe, room temperature, the t5 is typically 20ns. Therefore, I
believe the AD7738 should work with 10MHz SCLK, just keep the digital signal
capacitance to ground low (short tracks on PCB, low number of digital inputs
connected to the signal.)

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.