As per the absolute maximum rating table, as long as
- the analog input voltage is kept within ±21V and
- the analog input current below 10mA
no damage will be caused to the device. Independent on the device being powered or not.

KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
As per the absolute maximum rating table, as long as
no damage will be caused to the device. Independent on the device being powered or not.