As per the absolute maximum rating table, as long as
the analog input voltage is kept within ±21V and
the analog input current below 10mA
no damage will be caused to the device. Independent on…
KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the