AD73360AR: FAQ

  • Created
Was this helpful?
  • AD73360 timing questions

    Question I have some doubts over the timing of AD73360. In the datasheet, there is some description for SDOFS:(see figure1).Here it is mentioned that the period of SDOFS pulses would be 1/fsample,…
  • AD73360: Frequency response over sample rate

    Question What is the frequency response of AD73360 over different sample rates? Answer I have attached a spreadsheet for calculating the response based on sample rate. By selecting a sample rate…
  • AD73360: Grounding

    Question Please can you clarify the layout requirements for one of your parts? I cannot resolve the various requirements. The part in question is the AD73360 Analog Front End, and the question concerns…
  • AD73360: Lower limit of the MCLK

    Question Is there a lower limit to the frequency of the MCLK input? Answer There is no lower limit to the MCLK as long as it’s reasonable i.e. not in Hz etc. All the digital filters should scale with…
  • AD73360: SDOFS in figure 10

    Question The period of SDOFS pulses would be 1/fsample, just like Figure 10a. My question is for Figure 10b and 10c, what’s the period of SDOFS pulses? Answer The 1/f is when the sample is valid. The…
  • AD73360AR: DC performance

    Question I have a question about the AD73360 DC performance. I can't stabilise it's DC. DC is changed and I can't calibrate it I could get signal in 15 bit resolution without noise but the changing…
  • Long term drift for gain, Uref and FIT data

    Question The datasheet of AD73360 gives typical values only for some of the parameters.The information is back from 2000. Perhaps some min or max values have become available in the mean time which…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.