Article AD7192 ID Register

Question

Inquiry Description:The identification number for the AD7192 stored in the ID register is currently being read as 0xA0. Is this value fixed or likely to change in thefuture. I want to use the ID register value as fixed value for testing the PCB is functional.

Answer

The AD7192 has an ID of 0x80. The ID register is an 8-bit register. The register contains ID bits aswell as silicon revision bits. The 3 MSBsindicate the silicon revision while the 5 LSBS are the actual ID bits. There are no plans to revise the silicon. However, if the silicon was revised,the ‘8’ would increase to ‘A’ so the register would contain a value of 0xA8. To use thisregister, you can read all 8 bits. However, I suggest you only process the 5 LSBs. If the silicon were ever changed, the silicon revision would notaffect your system.
On powering up the hardware, I suggest that the you perform a reset (write 40 1s to the ADC). This reset sets all the on-chip registers to defaultvalues. So, rather than read the ID register, it may be better to read a larger register, for example, the mode register. This register will havemore bit variation than the ID register.


Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.