AD713: FAQ

  • Created
  • Updated
Was this helpful?
  • AD713

    Q I am currently working on a design requirement that needs to create an output of +10V and -10V at up to 20mA continuous (implies a 500ohm load). The device I have been considering for this application…
  • AD713: Output short circuit specifications

    Q I have got some questions about the output short circuit capability of AD713JR-16. In the datasheet (Rev. C) it is not clear said if the outputs are short circuit protected. The absolute maximum ratings…
  • AD713: Overvoltage at the inputs

    Q Has the AD713 internal protective diodes that allows voltages as high as 0.7 V beyond the supplies to be applied at the input of either terminal without causing damage. A In answer to your Question…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.