The specification of AD7403 only stipulates that the typical input common-mode voltage is -200~300mV, but it does not indicate the maximum value. However, in the process of use, I found that the input common-mode signal is 2V, which can still be used normally.So what is the maximum?