Power Integrity for High Performance Measurement Systems

    Increasing data rates driven by AI workloads and the evolution from 5G to emerging 6G standards are placing new demands on electronic test and measurement...
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
      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card! - Watts Going On? — The AI Power Delivery Quiz

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Reimagining Power for AI: Shaping the Future of AI Acceleration...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

EngineerZone
EngineerZone
High-Speed DACs
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
High-Speed DACs
  • Data Converters
High-Speed DACs
Documents External clock on the AD9164 FMC eval board
  • Q&A
  • File Uploads
  • FAQs/Docs
  • Members
  • Tags
  • Cancel

Products Mentioned

AD9164 Recommended for New Designs
The AD91641 is a high performance, 16-bit digital-to-analog converter (DAC) and direct digital synthesizer (DDS) that supports update rates to 6 GSPS....
Datasheet
AD9164 on Analog.com

Associated Drivers

AD9162 Recommended for New Designs
The AD9162 is a high performance, 16-bit digital-to-analog converter (DAC) that supports data rates to 6 GSPS. The DAC core is based on a quad-switch architecture...
Datasheet
AD9162 on Analog.com

Associated Drivers

Table of Contents
  • HIGH-SPEED DAC SUPPORT COMMUNITY
  • +Documents
  • +AD768ARZ: FAQ
  • +AD9102: FAQ
  • +AD9106: FAQ
  • +AD9115: FAQ
  • +AD9116: FAQ
  • +AD9117: FAQ
  • +AD9119: FAQ
  • +AD9122: FAQ
  • +AD9129: FAQ
  • +AD9135: FAQ
  • +AD9142A: FAQ
  • +AD9144: FAQ
  • +AD9146: FAQ
  • +AD9148: FAQ
  • +AD9286: FAQ
  • +AD9712: FAQ
  • +AD9716: FAQ
  • +AD9717: FAQ
  • +AD9726: FAQ
  • +AD9734: FAQ
  • +AD9736: FAQ
  • +AD9739: FAQ
  • +AD9739A: FAQ
  • +AD9742: FAQ
  • +AD9744: FAQ
  • +AD9747: FAQ
  • +AD9748: FAQ
  • +AD974: FAQ
  • +AD9763: FAQ
  • +AD9765: FAQ
  • +AD9767:FAQ
  • +AD976A: FAQ
  • +AD9774: FAQ
  • +AD9776: FAQ
  • +AD9777: FAQ
  • +AD9779: FAQ
  • +AD9779A: FAQ
  • +AD977: FAQ
  • +AD977A: FAQ
  • +AD9780: FAQ
  • +AD9783: FAQ
  • +AD9786: FAQ
  • +AD9788: FAQ
  • +AD9789: FAQ
  • +AD9161: FAQ
  • +AD9162: FAQ
  • -AD9164: FAQ
    • AD9162 eval board grounding/decoupling
    • AD9162 Temp Sensor Cal - Partial Start-Up Seq
    • AD9164 Chirp Waveforms
    • Are there IBIS-AMI models for the AD9162 and AD9164?
    • Can I MUX the data over the AD9162 JESD204B interface to share JESD pins between two digital chips?
    • External clock on the AD9164 FMC eval board
    • How do I create signals for the AD9161, AD9162, AD9163, AD9164 and ADS7-V2?
    • Is there a way to tweak the gain or output swing of the positive and/or negative branches of the DAC independently?
    • Time to change the AD9164 DAC clock frequency in NCO mode (DDS)
  • +AD9856: FAQ
  • +AD9857: FAQ
  • +AD9957: FAQ
  • +ADV7123: FAQ
  • +ADV7125: FAQ
  • +DPG3: FAQ
  • +MAX5189BEEI+: FAQ
  • +MAX5190BEEG+: FAQ
  • +MAX5868: FAQ
  • +MAX5871EXE+T: FAQ
  • +MAX5877EGK+D: FAQ
  • +MAX5880AUXF+: FAQ
  • +MAX5884EGM: FAQ
  • +MAX5891EGK+D: FAQ
  • +AD9136: FAQ
  • +AD9177: FAQ

External clock on the AD9164 FMC eval board

Question:

The external clock input on the AD9164-FMC-EBZ isn't working. ACE software selects to change it, but nothing happens on the eval board.

Resolution:

This is a known issue with boards that were produced near release time. The firmware programmed on the eval board does not toggle the control signal for the RF switch, making it such that the eval board will always use the on-board clock and won't use the external clock. This applies to AD9162-FMC-EBZ, AD9164-FMC-EBZ, and may apply to the AD9162-FMCB-EBZ and AD9164-FMCB-EBZ that have B-grade released parts loaded on them with date codes #1615. The issue applies to a small number of boards. The boards must be re-programmed at the factory with correct firmware. The customer should arrange return of the board with the local ADI support person (FAE or TSM), who should contact the ADI factory and arrange the return, re-program, and re-ship back to the customer.

Tags: KA-01002 AD9164-FMC-EBZ Standard High Speed D/A Converters high-speed dacs High Speed D/A Converters =30MSPS AD9162-FMC-EBZ external clock ad9164 ad9162 Show More