Open RAN 5G Radio Design: SDR SoCs for Energy-Efficient, Secure Deployments

    Building Secure and Energy‑Efficient 5G Networks with Software Defined Radios. The rapid evolution of 5G networks is driving new requirements for performance...
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
    • Power Integrity for High Performance Measurement Systems
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC Quizzes AQQ302 about Bang Gap Reference Generation

      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card! - Watts Going On? — The AI Power Delivery Quiz

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Reimagining Power for AI: Shaping the Future of AI Acceleration...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

EngineerZone
EngineerZone
High-Speed DACs
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
High-Speed DACs
  • Data Converters
High-Speed DACs
Documents Time to change the AD9164 DAC clock frequency in NCO mode (DDS)
  • Q&A
  • File Uploads
  • FAQs/Docs
  • Members
  • Tags
  • Cancel

Products Mentioned

AD9164 Recommended for New Designs
The AD91641 is a high performance, 16-bit digital-to-analog converter (DAC) and direct digital synthesizer (DDS) that supports update rates to 6 GSPS....
Datasheet
AD9164 on Analog.com

Associated Drivers

Table of Contents
  • HIGH-SPEED DAC SUPPORT COMMUNITY
  • +Documents
  • +AD768ARZ: FAQ
  • +AD9102: FAQ
  • +AD9106: FAQ
  • +AD9115: FAQ
  • +AD9116: FAQ
  • +AD9117: FAQ
  • +AD9119: FAQ
  • +AD9122: FAQ
  • +AD9129: FAQ
  • +AD9135: FAQ
  • +AD9142A: FAQ
  • +AD9144: FAQ
  • +AD9146: FAQ
  • +AD9148: FAQ
  • +AD9286: FAQ
  • +AD9712: FAQ
  • +AD9716: FAQ
  • +AD9717: FAQ
  • +AD9726: FAQ
  • +AD9734: FAQ
  • +AD9736: FAQ
  • +AD9739: FAQ
  • +AD9739A: FAQ
  • +AD9742: FAQ
  • +AD9744: FAQ
  • +AD9747: FAQ
  • +AD9748: FAQ
  • +AD974: FAQ
  • +AD9763: FAQ
  • +AD9765: FAQ
  • +AD9767:FAQ
  • +AD976A: FAQ
  • +AD9774: FAQ
  • +AD9776: FAQ
  • +AD9777: FAQ
  • +AD9779: FAQ
  • +AD9779A: FAQ
  • +AD977: FAQ
  • +AD977A: FAQ
  • +AD9780: FAQ
  • +AD9783: FAQ
  • +AD9786: FAQ
  • +AD9788: FAQ
  • +AD9789: FAQ
  • +AD9161: FAQ
  • +AD9162: FAQ
  • -AD9164: FAQ
    • AD9162 eval board grounding/decoupling
    • AD9162 Temp Sensor Cal - Partial Start-Up Seq
    • AD9164 Chirp Waveforms
    • Are there IBIS-AMI models for the AD9162 and AD9164?
    • Can I MUX the data over the AD9162 JESD204B interface to share JESD pins between two digital chips?
    • External clock on the AD9164 FMC eval board
    • How do I create signals for the AD9161, AD9162, AD9163, AD9164 and ADS7-V2?
    • Is there a way to tweak the gain or output swing of the positive and/or negative branches of the DAC independently?
    • Time to change the AD9164 DAC clock frequency in NCO mode (DDS)
  • +AD9856: FAQ
  • +AD9857: FAQ
  • +AD9957: FAQ
  • +ADV7123: FAQ
  • +ADV7125: FAQ
  • +DPG3: FAQ
  • +MAX5189BEEI+: FAQ
  • +MAX5190BEEG+: FAQ
  • +MAX5868: FAQ
  • +MAX5871EXE+T: FAQ
  • +MAX5877EGK+D: FAQ
  • +MAX5880AUXF+: FAQ
  • +MAX5884EGM: FAQ
  • +MAX5891EGK+D: FAQ
  • +AD9136: FAQ
  • +AD9177: FAQ

Time to change the AD9164 DAC clock frequency in NCO mode (DDS)

Question:

If I change the DACCLK on the AD9164 when using it as a DDS , what is the recovery time? How fast can I change sample clock and tuning word?

Answer:

The part would need to re-lock the DAC clock DLL and clear out the NCO phase accumulator, which happens in a few hundreds of clock cycles.

The safest method to do this would be to re-run the DAC start up sequence, which would add to the time to switch DAC clock frequency due to the series of SPI writes, but there is probably a subset of things that could be done, like perhaps disabling the DAC clock DLL, then re-enabling it, checking that the DLL re-locked, and then it should be good to go. This hasn't been characterized, but is a method the customer could try.

The speed to change NCO frequency is dependent on the number of SPI register writes and the SPI programming speed. At 100 MHz SPI writes, a single register write can be made in 240 ns, with an approximate 20 ns for the NCO to hop to the new frequency using phase discontinuous switch mode.

Tags: Standard High Speed D/A Converters KA-01001 high-speed dacs High Speed D/A Converters =30MSPS dds nco Barium ad9164 Show More