Open RAN 5G Radio Design: SDR SoCs for Energy-Efficient, Secure Deployments

    Building Secure and Energy‑Efficient 5G Networks with Software Defined Radios. The rapid evolution of 5G networks is driving new requirements for performance...
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
    • Power Integrity for High Performance Measurement Systems
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC Quizzes AQQ302 about Bang Gap Reference Generation

      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card! - Watts Going On? — The AI Power Delivery Quiz

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Reimagining Power for AI: Shaping the Future of AI Acceleration...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

EngineerZone
EngineerZone
High-Speed DACs
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
High-Speed DACs
  • Data Converters
High-Speed DACs
Documents What is the latency of the AD9789?
  • Q&A
  • File Uploads
  • FAQs/Docs
  • Members
  • Tags
  • Cancel

Products Mentioned

DAC86 Obsolete
Obsolete product page
DAC86 on Analog.com

dac100 Obsolete

dac100 on Analog.com

dac20 Obsolete
Obsolete Product
dac20 on Analog.com

DAC10 Not Recommended for New Designs
The DAC10 series of 10-bit monolithic multiplying digital-to-analog converters provide high speed performance and full-scale accuracy. Advanced circuit...
Datasheet
DAC10 on Analog.com

DAC16 Obsolete
The DAC16 is a 16-bit high speed current-output digital-to-analog converter with a settling time of 500 ns. A unique combination of low distortion, high...
DAC16 on Analog.com

DAC8562 Production
The DAC8562 is a complete, parallel input, 12-bit, voltage output DAC designed to operate from a single +5 volt supply. Built using a CBCMOS process, these...
Datasheet
DAC8562 on Analog.com

dac100s Production
The DAC-100 is a complete 10-bit resolution digital-to-analog converter constructed on two monolithic chips in a single 16-pin CERDIP. Featuring excellent...
Datasheet
dac100s on Analog.com

dac10df Production

dac10df on Analog.com

dac12qz Production

dac12qz on Analog.com

DAC8228 Production
The DAC-8228 is a dual 8-bit, voltage output, CMOS, D/A converter in a single chip. It was designed to drop into AD7528 / AD7628 sockets eliminating...
Datasheet
DAC8228 on Analog.com

dac1508a Obsolete
Obsolete Product
dac1508a on Analog.com

DAC02 Obsolete
This is an obsolete product.
DAC02 on Analog.com

DAC8413 Production
The DAC8412 / DAC8413 are quad, 12-bit voltage output DACs with readback capability. Built using a complementary BiCMOS process, these monolithic DACs...
Datasheet
DAC8413 on Analog.com

DAC8412 Production
The DAC8412 / DAC8413 are quad, 12-bit voltage output DACs with readback capability. Built using a complementary BiCMOS process, these monolithic DACs...
Datasheet
DAC8412 on Analog.com

dac1138 Obsolete
This is an obsolete product.
dac1138 on Analog.com

dac05 Obsolete
Obsolete Product
dac05 on Analog.com

dac03 Obsolete
Obsolete Product
dac03 on Analog.com

DAC8800 Production
The DAC-8800 Trim DACâ„¢ is designed to be a general purpose digitally controlled voltage adjustment device. The output voltage range can be independently...
Datasheet
DAC8800 on Analog.com

dac888 Obsolete

dac888 on Analog.com

DAC8841 Obsolete
The DAC-8841 provides eight general purpose digitally controlled voltage adjustment devices. The TRIMDACâ„¢ capability replaces the mechanical trimmer...
DAC8841 on Analog.com

DAC8420 Production
The DAC8420 is a quad, 12-bit voltage-output DAC with serial digital interface in a 16-lead package. Utilizing BiCMOS technology, this monolithic device...
Datasheet
DAC8420 on Analog.com

DAC8222 Not Recommended for New Designs
The DAC-8222 is a dual 12-bit, double-buffered, CMOS digital-to-analog converter. It has a 12-bit wide data port that allows a 12-bit word to be loaded...
Datasheet
DAC8222 on Analog.com

dac1132 Production

dac1132 on Analog.com

DAC8012 Obsolete
This is an obsolete product.
DAC8012 on Analog.com

DAC08S Production
The DAC-08 series of 8-bit monolithic digital-to-analog converters provide very high-speed performance coupled with low cost and outstanding applications...
Datasheet
DAC08S on Analog.com

DAC8512 Production
The DAC8512 is a complete serial input, 12-bit, voltage output digital-to-analog converter designed to operate from a single +5 V supply. It contains the...
Datasheet
DAC8512 on Analog.com

AD9789 Production
The AD9789 is a flexible QAM encoder/interpolator/upconverter combined with a high performance, 2400 MSPS, 14-bit RF digital-to-analog converter (DAC)...
Datasheet
AD9789 on Analog.com

dac1122 Production

dac1122 on Analog.com

DAC8143 Production
The DAC8143 is a 12-bit serial-input, daisy-chain digital-to-analog converter. It was designed for multiple serial DAC systems where serial daisy-chaining...
Datasheet
DAC8143 on Analog.com

dac1108 Production

dac1108 on Analog.com

DAC8426 Production
The DAC8426 is a complete quad voltage output D/A converter with internal reference. This product fits directly into any existing 7226 socket where the...
Datasheet
DAC8426 on Analog.com

DAC210 Obsolete
The DAC210 is a complete, monolithic 10-bit plus sign DAC with a ±10 V output. A precision voltage reference, a logic controlled polarity switch and output...
Datasheet
DAC210 on Analog.com

dac1009 Production

dac1009 on Analog.com

dac1106 Production

dac1106 on Analog.com

DAC8248 Not Recommended for New Designs
The DAC8248 is a dual 12-bit, double-buffered, CMOS digital-to-analog converter. It has an 8-bit wide input data port that interfaces directly with 8-bit...
Datasheet
DAC8248 on Analog.com

dac1423 Production

dac1423 on Analog.com

dac208 Obsolete
Obsolete Product
dac208 on Analog.com

DAC312 Not Recommended for New Designs
The DAC312 series of 12-bit multiplying digital-to-analog converters provide high speed with guaranteed performance to 0.012% differential nonlinearity...
Datasheet
DAC312 on Analog.com

dac1125 Production

dac1125 on Analog.com

dac8212 Obsolete
This is an obsolete product.
dac8212 on Analog.com

dac14qm Production

dac14qm on Analog.com

DAC8043 Not Recommended for New Designs
Newer Alternatives: NEW DESIGNS: AD5443 High Bandwidth CMOS 12-Bit Serial Interface Multiplying D/A Converter The DAC8043 is a high accuracy 12-bit CMOS...
Datasheet
DAC8043 on Analog.com

DAC1408 Production
Obsolete product page
DAC1408 on Analog.com

dac1146 Obsolete
Obsolete
dac1146 on Analog.com

DAC01 Obsolete
Obsolete product page
DAC01 on Analog.com

dac12m Production

dac12m on Analog.com

dac8m Production

dac8m on Analog.com

DAC8840 Obsolete
The DAC-8840 provides eight general purpose digitally controlled voltage adjustment devices. The TrimDAC® capability allows replacement of the mechanical...
Datasheet
DAC8840 on Analog.com

dac1136 Obsolete
This product is obsolete.
dac1136 on Analog.com

DAC8221 Not Recommended for New Designs
The DAC-8221 combines two identical 12-bit, multiplying, digital-to-analog converters into a single CMOS chip. This device is electrically similar to DAC...
Datasheet
DAC8221 on Analog.com

dac16qm Production

dac16qm on Analog.com

DAC8043A Production
The current-output DAC8043A provides a true 12-bit accurate (±1/2 LSB) digital-to-analog converter in compact 8-pin packages. Using a brand new circuit...
Datasheet
DAC8043A on Analog.com

dac10qm Obsolete

dac10qm on Analog.com

DAC8229 Not Recommended for New Designs
The DAC-8229 is a dual 8-bit, voltage output, multiplying CMOS D/A converter. Its reference iput accepts a ±2.5 V signal, inverts and delivers it to the...
Datasheet
DAC8229 on Analog.com

dac1117 Obsolete
This product is obsolete.
dac1117 on Analog.com

dac10zmda10z Production

dac10zmda10z on Analog.com

DAC8408 Not Recommended for New Designs
The DAC8408 is a monolithic quad 8-bit multiplying digital-to-analog CMOS converter. Each DAC has its own reference input, feedback resistor, and onboard...
Datasheet
DAC8408 on Analog.com

Table of Contents
  • HIGH-SPEED DAC SUPPORT COMMUNITY
  • +Documents
  • +AD768ARZ: FAQ
  • +AD9102: FAQ
  • +AD9106: FAQ
  • +AD9115: FAQ
  • +AD9116: FAQ
  • +AD9117: FAQ
  • +AD9119: FAQ
  • +AD9122: FAQ
  • +AD9129: FAQ
  • +AD9135: FAQ
  • +AD9142A: FAQ
  • +AD9144: FAQ
  • +AD9146: FAQ
  • +AD9148: FAQ
  • +AD9286: FAQ
  • +AD9712: FAQ
  • +AD9716: FAQ
  • +AD9717: FAQ
  • +AD9726: FAQ
  • +AD9734: FAQ
  • +AD9736: FAQ
  • +AD9739: FAQ
  • +AD9739A: FAQ
  • +AD9742: FAQ
  • +AD9744: FAQ
  • +AD9747: FAQ
  • +AD9748: FAQ
  • +AD974: FAQ
  • +AD9763: FAQ
  • +AD9765: FAQ
  • +AD9767:FAQ
  • +AD976A: FAQ
  • +AD9774: FAQ
  • +AD9776: FAQ
  • +AD9777: FAQ
  • +AD9779: FAQ
  • +AD9779A: FAQ
  • +AD977: FAQ
  • +AD977A: FAQ
  • +AD9780: FAQ
  • +AD9783: FAQ
  • +AD9786: FAQ
  • +AD9788: FAQ
  • -AD9789: FAQ
    • AD9789 start-up sequence--Is it okay to enable the mu controller first, then supply DAC clock?
    • AD9789: AD9789EBZ and AD9789-Mix-EBZ difference
    • Folded Harmonics
    • What is the latency of the AD9789?
  • +AD9161: FAQ
  • +AD9162: FAQ
  • +AD9164: FAQ
  • +AD9856: FAQ
  • +AD9857: FAQ
  • +AD9957: FAQ
  • +ADV7123: FAQ
  • +ADV7125: FAQ
  • +DPG3: FAQ
  • +MAX5189BEEI+: FAQ
  • +MAX5190BEEG+: FAQ
  • +MAX5868: FAQ
  • +MAX5871EXE+T: FAQ
  • +MAX5877EGK+D: FAQ
  • +MAX5880AUXF+: FAQ
  • +MAX5884EGM: FAQ
  • +MAX5891EGK+D: FAQ
  • +AD9136: FAQ
  • +AD9177: FAQ

What is the latency of the AD9789?

Q.

What is the latency of the AD9789?

-----------------------------------------------------------------------

A.

Define latency as the elapsed time from a sample clocked at the input to the AD9789 until the analog output begins changing. The latency of the AD9789 depends on which digital blocks are enabled in the datapath. The time can be approximated by using the calculation method provided below.

For each block in the table below that is enabled, take the latency number, and multiply it by the period of the clock listed in the units column to determine the latency through that block.  Sum all of the calculated latencies together to determine the latency through the device.  This method is not exact, but the approximation is sufficient for most applications.

block    latency    units

input       1           BR

QAM       1          BR

SRRC     44         BR/2

2x0        28         BR/4

2x1        13         BR/8

2x2        10         BR/16

2x3         5          BR/32

2x4         5          BR/64

RC          6          FS*16

DDS        5          FS*16

sum        3           FS*16

16x     144           FS

BR = period of baud rate clock

FS = period of DAC clock

Note that the highest latency values are calculated for those blocks that run at or close to the baud rate.

Tags: rfdac latency clock ad9789 dac
  • Share
  • History
  • More