What is the latency of AD9777,AD9775 and AD9773 16,14 and 12 bit DACs?
The answer is shown in the table below.
| AD977X Latency Table | |||||||||
| Interpolation Rate | Modulation Rate | Stage 1 Latency | Stage 2 Latency | Stage 3 Latency | Modulator Latency | Total Latency | |||
| 2 | 1 | 56 | 0 | 0 | 0 | 56 | |||
| 2 | 2 | 56 | 0 | 0 | 20 | 76 | |||
| 2 | 4 | 56 | 0 | 0 | 22 | 78 | |||
| 2 | 8 | 56 | 0 | 0 | 21 | 77 | |||
| 4 | 1 | 112 | 34 | 0 | 0 | 146 | |||
| 4 | 2 | 112 | 34 | 0 | 20 | 166 | |||
| 4 | 4 | 112 | 34 | 0 | 22 | 168 | |||
| 4 | 8 | 112 | 34 | 0 | 21 | 167 | |||
| 8 | 1 | 224 | 68 | 24 | 0 | 316 | |||
| 8 | 2 | 224 | 68 | 24 | 20 | 336 | |||
| 8 | 4 | 224 | 68 | 24 | 22 | 338 | |||
| 8 | 8 | 224 | 68 | 24 | 21 | 337 | |||
| Note: All latencies expressed in multiples of the DAC update rate, fDAC | |||||||||
This FAQ was generated from the following discussion: latency of the AD9777,5,3 DAC family