Join our webinar on the Quad Apollo Platform, a cutting-edge solution for accelerating high-performance digital beamforming. Discover the ADXBAND16EBZ...
1. Quote of this month: " When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his...
Important: Read the blog first . The quiz questions are all based on the content from the blog: Mature, Not Old! The Longevity of 4 – 20 mA New...
Whether you're debugging a stubborn camera link or designing a robust system from scratch, knowing where errors hide is half the battle. GMSL provides...
By Bryson Barney What if a single wire could carry both energy and information seamlessly—without either getting in the way? The future of connectivity...
Technical articles. Blogs. Videos. Your ADI content, all in one place.
Blurb About Content
At the AD9116 can run with DVDDIO=1.8V and AVDD = 3V?
Yes you can. The core can be run at an independent supply from the I/O.