Question
Some soldered jumpers on the AD9122 Evalboard are not as per default settings
mentioned in User Guide
Answer
Yes, there is an error in the User Guide (page 4).
The AD9122-M5375-EBZ and the AD9122-M5372-EBZ Evalboard User Guide states JP17
JP6 and JP4 and JP5 (pins 1&2)are connected by default (i.e. Figure 4(a)).
However, these jumpers are connected (pins2&3) by default according to 4(b).
The User Guide referred to is below:
ftp://ftp.analog.com/pub/HSSP_SW/HSCDAC/Documents/AD9122/AD9122%20Evaluation%20B
oard%20Quick%20Start%
20Guide.pdf
complete Documentation - Gerber Files, schmeatic etc...
ftp://ftp.analog.com/pub/HSSP_SW/HSCDAC/Documents/AD9122/