Power Management Fundamentals II Session 5: Deeper Look into Power Protection

    When is the best time to discover your power circuit needs protection? Let's explore the use of some input protection and control options like ideal diodes...
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
      1. Quote of this month: " When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Too Much Chatter and Not Enough Talk - Learn the Benefits...
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
    Achieving Power Over Data with RS-485 Transceivers

    By Bryson Barney What if a single wire could carry both energy and information seamlessly—without either getting in the way? The future of connectivity...

     

    ​​Functional Safety: A Driver of “Shift Left”​

    By Richard Obrien The key to faster, safer product development is to start smart - not catch up hard. In this blog, we’ll explore how the "Shift Left...

    Latest Blogs

    • The 5 Advantages of Hardware Fault Tolerance
    • The Power Problem Inside Every AI Breakthrough: Part 1 of 3
    • Simplifying Stability with EVAL-KW4503Z: Part 1 of 3
    • Energy Transfer Considerations in Isolated SMPS: Part 2 of 4
    • Automating LTspice .NOISE Measurements with .STEP and .MEAS Directives: Part 2 of 3
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
High-Speed DACs
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
High-Speed DACs
  • Data Converters
High-Speed DACs
Documents AD9129 - Mix-Mode function
  • Q&A
  • File Uploads
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • HIGH-SPEED DAC SUPPORT COMMUNITY
  • +Documents
  • +AD768ARZ: FAQ
  • +AD9102: FAQ
  • +AD9106: FAQ
  • +AD9115: FAQ
  • +AD9116: FAQ
  • +AD9117: FAQ
  • +AD9119: FAQ
  • +AD9122: FAQ
  • -AD9129: FAQ
    • AD9129 - Clock source and buffer recommendation
    • AD9129 - Compatible data generator ad9129
    • AD9129 - Highest RF output frequency spectrum supported
    • AD9129 - Mix-Mode function
    • AD9129 -  Clock source and buffer recommendation
    • AD9129 Analog Reference Plane
    • AD9129 datasheet clarifications
    • Evalboards use DAC "N" output and the datasheet uses the DAC "P" output. Which is correct?
  • +AD9135: FAQ
  • +AD9142A: FAQ
  • +AD9144: FAQ
  • +AD9146: FAQ
  • +AD9148: FAQ
  • +AD9286: FAQ
  • +AD9712: FAQ
  • +AD9716: FAQ
  • +AD9717: FAQ
  • +AD9726: FAQ
  • +AD9734: FAQ
  • +AD9736: FAQ
  • +AD9739: FAQ
  • +AD9739A: FAQ
  • +AD9742: FAQ
  • +AD9744: FAQ
  • +AD9747: FAQ
  • +AD9748: FAQ
  • +AD974: FAQ
  • +AD9763: FAQ
  • +AD9765: FAQ
  • +AD9767:FAQ
  • +AD976A: FAQ
  • +AD9774: FAQ
  • +AD9776: FAQ
  • +AD9777: FAQ
  • +AD9779: FAQ
  • +AD9779A: FAQ
  • +AD977: FAQ
  • +AD977A: FAQ
  • +AD9780: FAQ
  • +AD9783: FAQ
  • +AD9786: FAQ
  • +AD9788: FAQ
  • +AD9789: FAQ
  • +AD9161: FAQ
  • +AD9162: FAQ
  • +AD9164: FAQ
  • +AD9856: FAQ
  • +AD9857: FAQ
  • +AD9957: FAQ
  • +ADV7123: FAQ
  • +ADV7125: FAQ
  • +DPG3: FAQ
  • +MAX5189BEEI+: FAQ
  • +MAX5190BEEG+: FAQ
  • +MAX5868: FAQ
  • +MAX5871EXE+T: FAQ
  • +MAX5877EGK+D: FAQ
  • +MAX5880AUXF+: FAQ
  • +MAX5884EGM: FAQ
  • +MAX5891EGK+D: FAQ
  • +AD9136: FAQ
  • +AD9177: FAQ

AD9129 - Mix-Mode function

Question

What is the Mix-Mode function of the AD9129 and AD9119?

Answer

Mix-Mode enhances the DAC output power in the 2nd and 3rd Nyquist zone thus
increasing the usable output bandwidth of the device. In Mix-Mode the output is
effectively chopped at the DAC sample rate which has the effect of reducing the
power of the fundamental signal while increasing the power of the images
centered around the DAC sample rate. This improves the dynamic range of these
images. (See attachement)

Tags: high-speed dacs ad9129 3CVZ1254
  • Share
  • History
  • Cancel
 
Related Content
  • RE: AD9129-EBZ
    danf
    Hi, the customer can use the AD9129-EBZ to evaluate mix-mode. The performance may be slightly degraded compared to the performance of the mix-mode board. The main difference is the output balun/transformer...
  • RE: AD9129 mix mode and 2x interpolation
    danf
    In the block diagram, the 2x filter happens in the digital processing area, while the mix-mode operation happens at the DAC core. Because of this, both functions can be enabled or disabled independently...
  • AD9129 mix mode and 2x interpolation
    nauhzey
    What is the equivalent model when enable both mix mode and 2x interpolation? Based on the block diagram, the 2x interpolation will upsample the data by 2. Then the mix mode operation will simply change...
 
Related Content
  • RE: AD9129-EBZ
    danf
    Hi, the customer can use the AD9129-EBZ to evaluate mix-mode. The performance may be slightly degraded compared to the performance of the mix-mode board. The main difference is the output balun/transformer...
  • RE: AD9129 mix mode and 2x interpolation
    danf
    In the block diagram, the 2x filter happens in the digital processing area, while the mix-mode operation happens at the DAC core. Because of this, both functions can be enabled or disabled independently...
  • AD9129 mix mode and 2x interpolation
    nauhzey
    What is the equivalent model when enable both mix mode and 2x interpolation? Based on the block diagram, the 2x interpolation will upsample the data by 2. Then the mix mode operation will simply change...