Power Integrity for High Performance Measurement Systems

    Increasing data rates driven by AI workloads and the evolution from 5G to emerging 6G standards are placing new demands on electronic test and measurement...
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
      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read the Blog:  Simplified I/O: One Chip, Flexible Voltage Output, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Simplified I/O: One Chip, Flexible Voltage Outpu...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

EngineerZone
EngineerZone
High-Speed DACs
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
High-Speed DACs
  • Data Converters
High-Speed DACs
Documents AD9148: Unused channel / Unused pins
  • Q&A
  • File Uploads
  • FAQs/Docs
  • Members
  • Tags
  • Cancel

Products Mentioned

AD9148 Recommended for New Designs
The AD9148 is a quad, 16-bit, high dynamic range, digital-to-analog converter (DAC) that provides a sample rate of 1000 MSPS. These devices include features...
Datasheet
AD9148 on Analog.com

Table of Contents
  • HIGH-SPEED DAC SUPPORT COMMUNITY
  • +Documents
  • +AD768ARZ: FAQ
  • +AD9102: FAQ
  • +AD9106: FAQ
  • +AD9115: FAQ
  • +AD9116: FAQ
  • +AD9117: FAQ
  • +AD9119: FAQ
  • +AD9122: FAQ
  • +AD9129: FAQ
  • +AD9135: FAQ
  • +AD9142A: FAQ
  • +AD9144: FAQ
  • +AD9146: FAQ
  • -AD9148: FAQ
    • AD9148-EBZ + SDP-H1 Input Data Rate limitation
    • AD9148: Unused channel / Unused pins
  • +AD9286: FAQ
  • +AD9712: FAQ
  • +AD9716: FAQ
  • +AD9717: FAQ
  • +AD9726: FAQ
  • +AD9734: FAQ
  • +AD9736: FAQ
  • +AD9739: FAQ
  • +AD9739A: FAQ
  • +AD9742: FAQ
  • +AD9744: FAQ
  • +AD9747: FAQ
  • +AD9748: FAQ
  • +AD974: FAQ
  • +AD9763: FAQ
  • +AD9765: FAQ
  • +AD9767:FAQ
  • +AD976A: FAQ
  • +AD9774: FAQ
  • +AD9776: FAQ
  • +AD9777: FAQ
  • +AD9779: FAQ
  • +AD9779A: FAQ
  • +AD977: FAQ
  • +AD977A: FAQ
  • +AD9780: FAQ
  • +AD9783: FAQ
  • +AD9786: FAQ
  • +AD9788: FAQ
  • +AD9789: FAQ
  • +AD9161: FAQ
  • +AD9162: FAQ
  • +AD9164: FAQ
  • +AD9856: FAQ
  • +AD9857: FAQ
  • +AD9957: FAQ
  • +ADV7123: FAQ
  • +ADV7125: FAQ
  • +DPG3: FAQ
  • +MAX5189BEEI+: FAQ
  • +MAX5190BEEG+: FAQ
  • +MAX5868: FAQ
  • +MAX5871EXE+T: FAQ
  • +MAX5877EGK+D: FAQ
  • +MAX5880AUXF+: FAQ
  • +MAX5884EGM: FAQ
  • +MAX5891EGK+D: FAQ
  • +AD9136: FAQ
  • +AD9177: FAQ

AD9148: Unused channel / Unused pins

Question

The REFCLK/SYNC input does not need to be used. Can this input be left floating
or what termination is otherwise
required?
Also Port B is not being used, can these inputs be left floating?

Answer

You can float the REFCLK pins when you drive DACCLK. When you use only one of
the two channels, you can float the unused input.

For Port B, you just need to tie the Frame inputs to LVDS logic low if you are
not using Port B, they can cause problems when you float them.

Tags: Standard High Speed D/A Converters high-speed dacs High Speed D/A Converters =30MSPS ad9148 2DDX1644