Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
    • LEO Satcom: Application of RF, Mixed-Signal, & Beamforming ICs
    • 3 Real World Methods to Make Your Power Supply More Intelligent
    • Revolutionizing Flow Cytometry: 20-Bit Precision Signal Chain
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC's Quiz AQQ300 about Divisibility by 6

      1. Quote of the month: " Friendship is like money - easier made than kept " - Samuel Butler 2. New quiz AQQ300 about a divisibility by 6 puzzle ...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card

      Important: Read the blog first . The quiz questions are all based on the content from the blog: The Power Problem Inside Every AI Breakthrough Everyone...
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
    Clock Tree Design and Why “PLL Locked” Is Not Enough

    In high-performance RF systems, clocking architecture is a foundational element that directly governs signal integrity, synchronization, and overall system...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    The Right Switch-Mode Power Supply Control Scheme

    This article compares three switch-mode power supply control schemescurrent-mode control, voltage-mode control, and hysteretic-mode control to guide engineers...

EngineerZone
EngineerZone
High-Speed DACs
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
High-Speed DACs
  • Data Converters
High-Speed DACs
Documents AD9726: Interface with the AD600
  • Q&A
  • File Uploads
  • FAQs/Docs
  • Members
  • Tags
  • Cancel

Products Mentioned

AD9726 Not Recommended for New Designs
The AD9726 is a 16-bit high performance LVDS DAC that offers exceptional noise and spurious performance and true 16-bit dc linearity. Manufactured on a...
Datasheet
AD9726 on Analog.com

AD600 Production
The AD600/AD602 dual channel, low noise, variable gain amplifiers are optimized for use in ultrasound imaging systems, but are applicable to any application...
Datasheet
AD600 on Analog.com

Table of Contents
  • HIGH-SPEED DAC SUPPORT COMMUNITY
  • +Documents
  • +AD768ARZ: FAQ
  • +AD9102: FAQ
  • +AD9106: FAQ
  • +AD9115: FAQ
  • +AD9116: FAQ
  • +AD9117: FAQ
  • +AD9119: FAQ
  • +AD9122: FAQ
  • +AD9129: FAQ
  • +AD9135: FAQ
  • +AD9142A: FAQ
  • +AD9144: FAQ
  • +AD9146: FAQ
  • +AD9148: FAQ
  • +AD9286: FAQ
  • +AD9712: FAQ
  • +AD9716: FAQ
  • +AD9717: FAQ
  • -AD9726: FAQ
    • AD9726: Interface with the AD600
    • AD9726_Iout equation error
  • +AD9734: FAQ
  • +AD9736: FAQ
  • +AD9739: FAQ
  • +AD9739A: FAQ
  • +AD9742: FAQ
  • +AD9744: FAQ
  • +AD9747: FAQ
  • +AD9748: FAQ
  • +AD974: FAQ
  • +AD9763: FAQ
  • +AD9765: FAQ
  • +AD9767:FAQ
  • +AD976A: FAQ
  • +AD9774: FAQ
  • +AD9776: FAQ
  • +AD9777: FAQ
  • +AD9779: FAQ
  • +AD9779A: FAQ
  • +AD977: FAQ
  • +AD977A: FAQ
  • +AD9780: FAQ
  • +AD9783: FAQ
  • +AD9786: FAQ
  • +AD9788: FAQ
  • +AD9789: FAQ
  • +AD9161: FAQ
  • +AD9162: FAQ
  • +AD9164: FAQ
  • +AD9856: FAQ
  • +AD9857: FAQ
  • +AD9957: FAQ
  • +ADV7123: FAQ
  • +ADV7125: FAQ
  • +DPG3: FAQ
  • +MAX5189BEEI+: FAQ
  • +MAX5190BEEG+: FAQ
  • +MAX5868: FAQ
  • +MAX5871EXE+T: FAQ
  • +MAX5877EGK+D: FAQ
  • +MAX5880AUXF+: FAQ
  • +MAX5884EGM: FAQ
  • +MAX5891EGK+D: FAQ
  • +AD9136: FAQ
  • +AD9177: FAQ

AD9726: Interface with the AD600

Question

AD9726 DAC output is differential and AD600 signal inputs are not fully
differential. Can AD9726 drive directly AD600 (differential), or do I have to
do converson with OP AMP?
Output of AD600 is not differential (A1CM and A2CM connected to GND). Do you
have reference desing?

Answer

The AD600 has a gain range of 0 dB to +40 dB (X1 to X100). If you are using the
AD600 with +/- 5V supplies your maximum output is 6V pk-pk, which is (very
approximately) 2 V rms. The AD9726 delivers 40 mA pk-pk (i.e. differential
outputs with 0-20 mA flowing in each in antiphase) and I assume that you wish
the AD600 to deliver 20 mV to 2 V rms, by variation of its gain control, with
the AD9726 programmed to full-scale digital input. Unless you are working at
the maximum output frequency of the AD9726 you will not need to run the AD9726
at such a high current, but you should not run it at such a low current that
feeding that current into 100 Ohms gives you your 20 mV rms.

You will therefore need to arrange for the AD9726 run at a lower output current
by use of an appropriate resistor on the FSADJ pin and to deliver 20 mV rms to
the AD600.

I cannot see any need for an amplifier here, you have ample signal to spare -
you can do a perfectly adequate job with resistors or with a transformer.

Assume that your programmed total output current is X mA, then the pk-pk output
current is 2X mA and the rms. output current is X/SqRoot2 mA.

The simplest solution seems to me to be to ground one output and allow
X/(2.SqRoot2) mA rms to flow from the other output in a grounded load resistor
R to give 20 mV rms. This calls for R = (40.SqRoot2/X) Ohms. Couple this
voltage to the AD600 input with a capacitor to provide DC isolation (otherwise
the AD600 output will have a DC bias). The value of R may need to be altered to
compensate for the parallel Zin of the AD600 (100 Ohms) but in practice this
error may be trimmed out in other ways.

If you wish the above circuit to be balanced you can terminate the unused
AD9726 output with another resistance of R instead of simply grounding it. NOTE
THAT YOU MUST NOT LEAVE THIS UNUSED OUTPUT OPEN CIRCUIT.

Instead of using unbalanced coupling you can use a broadband transformer with a
centre-taped primary. The centre tap is grounded and the differential outputs
of the AD9726 feed opposite ends of the primary. The secondary is connected to
the AD600 AinHi and to ground. AinLO of the AD600 is also grounded. With this
arrangement it is necessary to shunt either the primary or the secondary of the
transformer with a resistor to prevent the AD600 input signal from being too
large. The value of the resistor will depend on the AD9726 output current
programmed and the transformer ratio.

Tags: Analog Control Variable Gain Amplifiers (VGAs) Standard High Speed D/A Converters high-speed dacs 5DBN5357 ad9726 High Speed D/A Converters =30MSPS ad600 Variable Gain Amplifiers (VGA) Show More