Accelerate RF Subsystem Integration with COTS SoMs and Phased Array Solutions. As building a subsystem from early prototype to full deployment is never...
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
      1. Quote of the month: " Friendship is like money - easier made than kept " - Samuel Butler 2. New quiz AQQ300 about a divisibility by 6 puzzle ...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Taming the AI Power Storm: Part 2 of 3 Test your...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Calibration Implementation Techniques for Multichannel Phased Array Subsystems

    Learn about phase-calibration techniques used for characterizing a 16 transmit and 16 receive X-band phased array subsystem based on a mixed-signal front...

EngineerZone
EngineerZone
High-Speed DACs
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
High-Speed DACs
  • Data Converters
High-Speed DACs
Documents Impedance matching when AD9717 or AD9779A interfaced with ADL5375
  • Q&A
  • File Uploads
  • FAQs/Docs
  • Members
  • Tags
  • Cancel

Products Mentioned

ADL5375 Production
The ADL5375 is a broadband quadrature modulator designed for operation from 400 MHz to 6 GHz. Its excellent phase accuracy and amplitude balance enable...
Datasheet
ADL5375 on Analog.com

AD9779A Production
The AD9776A / AD9778A / AD9779A are dual, 12-/14-/16-bit, high dynamic range digital-to-analog converters (DACs) that provide a sample rate of 1 GSPS...
Datasheet
AD9779A on Analog.com

AD9717 Production
The AD9714 / AD9715 / AD9716 / AD9717 are pin-compatible, dual, 8-/10-/12-/14-bit, low power digital-to-analog converters (DACs) that provide a sample...
Datasheet
AD9717 on Analog.com

Table of Contents
  • HIGH-SPEED DAC SUPPORT COMMUNITY
  • +Documents
  • +AD768ARZ: FAQ
  • +AD9102: FAQ
  • +AD9106: FAQ
  • +AD9115: FAQ
  • +AD9116: FAQ
  • +AD9117: FAQ
  • +AD9119: FAQ
  • +AD9122: FAQ
  • +AD9129: FAQ
  • +AD9135: FAQ
  • +AD9142A: FAQ
  • +AD9144: FAQ
  • +AD9146: FAQ
  • +AD9148: FAQ
  • +AD9286: FAQ
  • +AD9712: FAQ
  • +AD9716: FAQ
  • +AD9717: FAQ
  • +AD9726: FAQ
  • +AD9734: FAQ
  • +AD9736: FAQ
  • +AD9739: FAQ
  • +AD9739A: FAQ
  • +AD9742: FAQ
  • +AD9744: FAQ
  • +AD9747: FAQ
  • +AD9748: FAQ
  • +AD974: FAQ
  • +AD9763: FAQ
  • +AD9765: FAQ
  • +AD9767:FAQ
  • +AD976A: FAQ
  • +AD9774: FAQ
  • +AD9776: FAQ
  • +AD9777: FAQ
  • +AD9779: FAQ
  • -AD9779A: FAQ
    • Impedance matching when AD9717 or AD9779A interfaced with ADL5375
  • +AD977: FAQ
  • +AD977A: FAQ
  • +AD9780: FAQ
  • +AD9783: FAQ
  • +AD9786: FAQ
  • +AD9788: FAQ
  • +AD9789: FAQ
  • +AD9161: FAQ
  • +AD9162: FAQ
  • +AD9164: FAQ
  • +AD9856: FAQ
  • +AD9857: FAQ
  • +AD9957: FAQ
  • +ADV7123: FAQ
  • +ADV7125: FAQ
  • +DPG3: FAQ
  • +MAX5189BEEI+: FAQ
  • +MAX5190BEEG+: FAQ
  • +MAX5868: FAQ
  • +MAX5871EXE+T: FAQ
  • +MAX5877EGK+D: FAQ
  • +MAX5880AUXF+: FAQ
  • +MAX5884EGM: FAQ
  • +MAX5891EGK+D: FAQ
  • +AD9136: FAQ
  • +AD9177: FAQ

Impedance matching when AD9717 or AD9779A interfaced with ADL5375

Question

Can you confirm why I need to use 500ohm or 50ohm impedance matching for the
AD9717 and AD9779A interfaced to ADL5375.
Sorry for that basic questions, but I am from the digital world.

 

Answer

Remember, that the AD9717's and AD9779A's output and ADL5375's input
common-mode bias levels are both 500mV and hence do not require voltage
shifting circuitry.

With regards to the AD9717, whose fullscale output current=2mA, then to obtain
500mV bias on the output the voltage can vary from 0 to 1V for single-ended.
Therefore, the corresponding resistance (RBIP, RBIN) = 1V/2mA = 500ohms.

In the case of the AD9779A, the fullscale output current=20mA and to have an
output single-end voltage from 0 to 1V, then the corresponding resistance
(RBIP, RBIN) = 1V/20mA = 50ohms.

Refer to Figure 59 in the ADL5375's RevB datasheet for further details

Tags: Standard High Speed D/A Converters high-speed dacs 2DTR1924 I/Q Modulators ad9779a adl5375 High Speed D/A Converters =30MSPS ad9717 I/Q Modulators and Demodulators Show More
  • Share
  • History
  • Cancel
 
Related Content
  • RE: AD9779A with ADL5385
    zpandangan
    Hi srdjan1 , There are four parts to consider when designing an interface circuit between the AD9779A and ADL5385: Bias-Setting Resistors. These resistors establish the bias level from the DAC to...
  • RE: More Questions About the AD9161
    hkumar
    Hi Randy, On the ADL5375 side of things: To get a single-side band output, the inputs to ADL5375, I and Q, need to be quadrature in phase, that is, 90 degrees apart. Also, the baseband input bias levels...
  • RE: Getting pixel data from the ADV7611 into a DAC
    hkumar
    Depending on your application, could you perhaps use a mixer to upconvert the RGB data? If you have to use the ADL5375, as edo mentioned, the I and Q inputs need to be in quadrature phase - 90 degrees...
 
Related Content
  • RE: AD9779A with ADL5385
    zpandangan
    Hi srdjan1 , There are four parts to consider when designing an interface circuit between the AD9779A and ADL5385: Bias-Setting Resistors. These resistors establish the bias level from the DAC to...
  • RE: More Questions About the AD9161
    hkumar
    Hi Randy, On the ADL5375 side of things: To get a single-side band output, the inputs to ADL5375, I and Q, need to be quadrature in phase, that is, 90 degrees apart. Also, the baseband input bias levels...
  • RE: Getting pixel data from the ADV7611 into a DAC
    hkumar
    Depending on your application, could you perhaps use a mixer to upconvert the RGB data? If you have to use the ADL5375, as edo mentioned, the I and Q inputs need to be in quadrature phase - 90 degrees...