Open RAN 5G Radio Design: SDR SoCs for Energy-Efficient, Secure Deployments

    Building Secure and Energy‑Efficient 5G Networks with Software Defined Radios. The rapid evolution of 5G networks is driving new requirements for performance...
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
    • Power Integrity for High Performance Measurement Systems
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC Quizzes AQQ302 about Bang Gap Reference Generation

      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card! - Watts Going On? — The AI Power Delivery Quiz

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Reimagining Power for AI: Shaping the Future of AI Acceleration...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

EngineerZone
EngineerZone
High-Speed DACs
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
High-Speed DACs
  • Data Converters
High-Speed DACs
Documents How do I create signals for the AD9161, AD9162, AD9163, AD9164 and ADS7-V2?
  • Q&A
  • File Uploads
  • FAQs/Docs
  • Members
  • Tags
  • Cancel

Products Mentioned

AD9164 Recommended for New Designs
The AD91641 is a high performance, 16-bit digital-to-analog converter (DAC) and direct digital synthesizer (DDS) that supports update rates to 6 GSPS....
Datasheet
AD9164 on Analog.com

Associated Drivers

AD9163 Recommended for New Designs
The AD91631 is a high performance, 16-bit digital-to-analog converter (DAC) that supports data rates to 6 GSPS. The DAC core is based on a quad-switch...
Datasheet
AD9163 on Analog.com

Associated Drivers

AD9161 Recommended for New Designs
The AD9161 is a high performance, 11-bit digital-to-analog converter (DAC) that supports data rates to 6 GSPS. The DAC core is based on a quad-switch architecture...
Datasheet
AD9161 on Analog.com

Associated Drivers

AD9162 Recommended for New Designs
The AD9162 is a high performance, 16-bit digital-to-analog converter (DAC) that supports data rates to 6 GSPS. The DAC core is based on a quad-switch architecture...
Datasheet
AD9162 on Analog.com

Associated Drivers

Table of Contents
  • HIGH-SPEED DAC SUPPORT COMMUNITY
  • +Documents
  • +AD768ARZ: FAQ
  • +AD9102: FAQ
  • +AD9106: FAQ
  • +AD9115: FAQ
  • +AD9116: FAQ
  • +AD9117: FAQ
  • +AD9119: FAQ
  • +AD9122: FAQ
  • +AD9129: FAQ
  • +AD9135: FAQ
  • +AD9142A: FAQ
  • +AD9144: FAQ
  • +AD9146: FAQ
  • +AD9148: FAQ
  • +AD9286: FAQ
  • +AD9712: FAQ
  • +AD9716: FAQ
  • +AD9717: FAQ
  • +AD9726: FAQ
  • +AD9734: FAQ
  • +AD9736: FAQ
  • +AD9739: FAQ
  • +AD9739A: FAQ
  • +AD9742: FAQ
  • +AD9744: FAQ
  • +AD9747: FAQ
  • +AD9748: FAQ
  • +AD974: FAQ
  • +AD9763: FAQ
  • +AD9765: FAQ
  • +AD9767:FAQ
  • +AD976A: FAQ
  • +AD9774: FAQ
  • +AD9776: FAQ
  • +AD9777: FAQ
  • +AD9779: FAQ
  • +AD9779A: FAQ
  • +AD977: FAQ
  • +AD977A: FAQ
  • +AD9780: FAQ
  • +AD9783: FAQ
  • +AD9786: FAQ
  • +AD9788: FAQ
  • +AD9789: FAQ
  • +AD9161: FAQ
  • +AD9162: FAQ
  • -AD9164: FAQ
    • AD9162 eval board grounding/decoupling
    • AD9162 Temp Sensor Cal - Partial Start-Up Seq
    • AD9164 Chirp Waveforms
    • Are there IBIS-AMI models for the AD9162 and AD9164?
    • Can I MUX the data over the AD9162 JESD204B interface to share JESD pins between two digital chips?
    • External clock on the AD9164 FMC eval board
    • How do I create signals for the AD9161, AD9162, AD9163, AD9164 and ADS7-V2?
    • Is there a way to tweak the gain or output swing of the positive and/or negative branches of the DAC independently?
    • Time to change the AD9164 DAC clock frequency in NCO mode (DDS)
  • +AD9856: FAQ
  • +AD9857: FAQ
  • +AD9957: FAQ
  • +ADV7123: FAQ
  • +ADV7125: FAQ
  • +DPG3: FAQ
  • +MAX5189BEEI+: FAQ
  • +MAX5190BEEG+: FAQ
  • +MAX5868: FAQ
  • +MAX5871EXE+T: FAQ
  • +MAX5877EGK+D: FAQ
  • +MAX5880AUXF+: FAQ
  • +MAX5884EGM: FAQ
  • +MAX5891EGK+D: FAQ
  • +AD9136: FAQ
  • +AD9177: FAQ

How do I create signals for the AD9161, AD9162, AD9163, AD9164 and ADS7-V2?

Question:

I am using the AD9163-FMCC-EBZ and ADS7-V2. How do I generate signals as I want (sines with different freqs. combinations) using the ADS7-V2 software? Can I use my own application (labview, matlab, etc) for this purpose? In other words, how can I load my digital words in the ADS7-V2 to obtain an analog signal in the AD9163 output?

Resolution:

You can use DAC Software Suite, which includes the DPG Downloader, to create many standard communication signal waveforms. You can also create your own waveforms in Matlab or any other software, save them, and import them into DPG Downloader and play them. This method is described in the User Guide on the Analog Devices Wiki site here: https://wiki.analog.com/resources/eval/dpg/ad916x-fmcx-ebz#using_external_files

Tags: KA-01070 Standard High Speed D/A Converters ad9161 high-speed dacs High Speed D/A Converters =30MSPS ads7-v2 signals matlab ad9163 frequency DPG Downloader ad9164 ad9162 Show More