Open RAN 5G Radio Design: SDR SoCs for Energy-Efficient, Secure Deployments

    Building Secure and Energy‑Efficient 5G Networks with Software Defined Radios. The rapid evolution of 5G networks is driving new requirements for performance...
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
    • Power Integrity for High Performance Measurement Systems
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC Quizzes AQQ302 about Bang Gap Reference Generation

      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card! - Watts Going On? — The AI Power Delivery Quiz

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Reimagining Power for AI: Shaping the Future of AI Acceleration...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

EngineerZone
EngineerZone
High-Speed DACs
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
High-Speed DACs
  • Data Converters
High-Speed DACs
Documents AD9164 Chirp Waveforms
  • Q&A
  • File Uploads
  • FAQs/Docs
  • Members
  • Tags
  • Cancel

Products Mentioned

AD9164 Recommended for New Designs
The AD91641 is a high performance, 16-bit digital-to-analog converter (DAC) and direct digital synthesizer (DDS) that supports update rates to 6 GSPS....
Datasheet
AD9164 on Analog.com

Associated Drivers

Table of Contents
  • HIGH-SPEED DAC SUPPORT COMMUNITY
  • +Documents
  • +AD768ARZ: FAQ
  • +AD9102: FAQ
  • +AD9106: FAQ
  • +AD9115: FAQ
  • +AD9116: FAQ
  • +AD9117: FAQ
  • +AD9119: FAQ
  • +AD9122: FAQ
  • +AD9129: FAQ
  • +AD9135: FAQ
  • +AD9142A: FAQ
  • +AD9144: FAQ
  • +AD9146: FAQ
  • +AD9148: FAQ
  • +AD9286: FAQ
  • +AD9712: FAQ
  • +AD9716: FAQ
  • +AD9717: FAQ
  • +AD9726: FAQ
  • +AD9734: FAQ
  • +AD9736: FAQ
  • +AD9739: FAQ
  • +AD9739A: FAQ
  • +AD9742: FAQ
  • +AD9744: FAQ
  • +AD9747: FAQ
  • +AD9748: FAQ
  • +AD974: FAQ
  • +AD9763: FAQ
  • +AD9765: FAQ
  • +AD9767:FAQ
  • +AD976A: FAQ
  • +AD9774: FAQ
  • +AD9776: FAQ
  • +AD9777: FAQ
  • +AD9779: FAQ
  • +AD9779A: FAQ
  • +AD977: FAQ
  • +AD977A: FAQ
  • +AD9780: FAQ
  • +AD9783: FAQ
  • +AD9786: FAQ
  • +AD9788: FAQ
  • +AD9789: FAQ
  • +AD9161: FAQ
  • +AD9162: FAQ
  • -AD9164: FAQ
    • AD9162 eval board grounding/decoupling
    • AD9162 Temp Sensor Cal - Partial Start-Up Seq
    • AD9164 Chirp Waveforms
    • Are there IBIS-AMI models for the AD9162 and AD9164?
    • Can I MUX the data over the AD9162 JESD204B interface to share JESD pins between two digital chips?
    • External clock on the AD9164 FMC eval board
    • How do I create signals for the AD9161, AD9162, AD9163, AD9164 and ADS7-V2?
    • Is there a way to tweak the gain or output swing of the positive and/or negative branches of the DAC independently?
    • Time to change the AD9164 DAC clock frequency in NCO mode (DDS)
  • +AD9856: FAQ
  • +AD9857: FAQ
  • +AD9957: FAQ
  • +ADV7123: FAQ
  • +ADV7125: FAQ
  • +DPG3: FAQ
  • +MAX5189BEEI+: FAQ
  • +MAX5190BEEG+: FAQ
  • +MAX5868: FAQ
  • +MAX5871EXE+T: FAQ
  • +MAX5877EGK+D: FAQ
  • +MAX5880AUXF+: FAQ
  • +MAX5884EGM: FAQ
  • +MAX5891EGK+D: FAQ
  • +AD9136: FAQ
  • +AD9177: FAQ

AD9164 Chirp Waveforms

Question:

Do you have a user’s guide for creating chirp waveforms using the AD9164 with the pattern generator board?

Resolution:

There is no documentation on the chirp generator in DPG Downloader. The usage of the generator is straightforward: set a start frequency, a stop frequency, and a data rate, and the vector spreads that frequency change over the record length.

Tags: Standard High Speed D/A Converters high-speed dacs AD9164 Chirp Waveforms DPG Downloader High Speed D/A Converters =30MSPS KA-01048 ad9164 Show More
  • Share
  • History
  • Cancel
 
Related Content
  • chirp
    chirp
    $core_v2_language.Truncate($item.HtmlDescription('Web'), 200, "...")
  • DPG-Lite : Can I adjust the phase of Chirp waveform?
    y_suzuki
    Hello, I have a question about generating a chirp waveform using DPG-Lite. Our customer wants to generate a complex(I/Q) chirp waveform but the function of "Chirp" in "Add Generated Waveform" can not generate...
  • RE: AD9910 positive chirp with EVB
    mcee
    Hi, In order to have your desired frequency chirp, the no-dwell high bit should be high. While the no-dwell high bit is set to high, the following are the answers to your questions: 1. The DROVER...
 
Related Content
  • chirp
    chirp
    $core_v2_language.Truncate($item.HtmlDescription('Web'), 200, "...")
  • DPG-Lite : Can I adjust the phase of Chirp waveform?
    y_suzuki
    Hello, I have a question about generating a chirp waveform using DPG-Lite. Our customer wants to generate a complex(I/Q) chirp waveform but the function of "Chirp" in "Add Generated Waveform" can not generate...
  • RE: AD9910 positive chirp with EVB
    mcee
    Hi, In order to have your desired frequency chirp, the no-dwell high bit should be high. While the no-dwell high bit is set to high, the following are the answers to your questions: 1. The DROVER...