Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC Quiz AQQ299 about Opamp open looop gain and LTspice (a kind proposal from Al Butvidas)

      1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits next to you and says 'wasn't that...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Understanding Voltage Domain Isolation in Field-Bus...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    PSM Integration for Enhanced Module Solutions in 48 V Data Centers

    The integration of the LTC2971 into quarter brick solutions for 48 V data centers enhances monitoring, control, and reliability by providing high precision...

EngineerZone
EngineerZone
High-Speed DACs
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
High-Speed DACs
  • Data Converters
High-Speed DACs
Documents ADV7123: Output with no power applied
  • Q&A
  • File Uploads
  • FAQs/Docs
  • Members
  • Tags
  • Cancel

Products Mentioned

ADV7125 Production
The ADV7125 (ADV®) is a triple high speed, digital-to-analog converter (DAC) on a single monolithic chip. It consists of three high speed, 8-bit video...
Datasheet
ADV7125 on Analog.com

ADV7123 Production
The ADV7123 (ADV®) is a triple high speed, digital-to-analog converter on a single monolithic chip. It consists of three high speed, 10-bit, video DACs...
Datasheet
ADV7123 on Analog.com

AD589 Not Recommended for New Designs
The AD589 is a two-terminal, low cost, temperature compensated bandgap voltage reference which provides a fixed 1.23 V output voltage for input currents...
Datasheet
AD589 on Analog.com

AD589S Production
The AD589 is a two-terminal, temperature compensated bandgap voltage reference which provides a fixed 1.23 V output voltage for input currents between...
Datasheet
AD589S on Analog.com

Table of Contents
  • HIGH-SPEED DAC SUPPORT COMMUNITY
  • +Documents
  • +AD768ARZ: FAQ
  • +AD9102: FAQ
  • +AD9106: FAQ
  • +AD9115: FAQ
  • +AD9116: FAQ
  • +AD9117: FAQ
  • +AD9119: FAQ
  • +AD9122: FAQ
  • +AD9129: FAQ
  • +AD9135: FAQ
  • +AD9142A: FAQ
  • +AD9144: FAQ
  • +AD9146: FAQ
  • +AD9148: FAQ
  • +AD9286: FAQ
  • +AD9712: FAQ
  • +AD9716: FAQ
  • +AD9717: FAQ
  • +AD9726: FAQ
  • +AD9734: FAQ
  • +AD9736: FAQ
  • +AD9739: FAQ
  • +AD9739A: FAQ
  • +AD9742: FAQ
  • +AD9744: FAQ
  • +AD9747: FAQ
  • +AD9748: FAQ
  • +AD974: FAQ
  • +AD9763: FAQ
  • +AD9765: FAQ
  • +AD9767:FAQ
  • +AD976A: FAQ
  • +AD9774: FAQ
  • +AD9776: FAQ
  • +AD9777: FAQ
  • +AD9779: FAQ
  • +AD9779A: FAQ
  • +AD977: FAQ
  • +AD977A: FAQ
  • +AD9780: FAQ
  • +AD9783: FAQ
  • +AD9786: FAQ
  • +AD9788: FAQ
  • +AD9789: FAQ
  • +AD9161: FAQ
  • +AD9162: FAQ
  • +AD9164: FAQ
  • +AD9856: FAQ
  • +AD9857: FAQ
  • +AD9957: FAQ
  • -ADV7123: FAQ
    • ADV7123 - Vref minimum and maximum specification is missing in the datasheet
    • ADV7123 EVB
    • ADV7123: Analog O/P values
    • ADV7123: Driving terminated video lines
    • ADV7123: Output with no power applied
  • +ADV7125: FAQ
  • +DPG3: FAQ
  • +MAX5189BEEI+: FAQ
  • +MAX5190BEEG+: FAQ
  • +MAX5868: FAQ
  • +MAX5871EXE+T: FAQ
  • +MAX5877EGK+D: FAQ
  • +MAX5880AUXF+: FAQ
  • +MAX5884EGM: FAQ
  • +MAX5891EGK+D: FAQ
  • +AD9136: FAQ
  • +AD9177: FAQ

ADV7123: Output with no power applied

Question

My question concerns DAC ADV7123.
On our board we use EP9315 (Cirrus Logic) as a processor. It contains video
interface connected to DAC. Digital level is 0 to 3,3V. DAC is powered from 5V,
also has external reference voltage AD589, pulled by 3.9k resistor from Vref to
5V. Rset = 430 ohm, COMP capacitor = 100nF. After few months some PCB's back to
us with ADV7123 damage. Picture is gray but it can be see on it an mosaic of
proper picture. What is the reason of this kind of damage? I have also a few
questions.
1. How ADV7123 detects working with external reverence voltage?
2. We use only 8 bit for each channel. Does 2 MSB's each channel should be
tied to GND ?
3. ADV7123 works without power supply - it is possible that the power is
supplies by digital inputs of RGB ?

Answer

1. You can use an external Voltage reference or as we have seen in some low
cost instances a voltage divider network with approximately 10Kohm values. For
low clock speed operation the internal voltage reference should be adequate.

2. Yes (connect to ground) , or use the ADV7125 pin compatible 8-bit version of
the IC.

3. It is advised to run the part within the specified operating limits.
Non standard supplies may switch on the protection diodes and although the part
may operate damage can result.

When you have no power supply (VAA=0 volts) , the voltage applied to the
digital pins needs to be within the range -0.5 to +0.5 volts.
Otherwise you will forward bias the built in ESD protection diodes.

See the Absolute maximum ratings on page 8 of the ADV7123 datasheet.

Tags: Standard High Speed D/A Converters high-speed dacs 5D4W2155 Shunt Voltage References High Speed D/A Converters =30MSPS ad589 voltage references adv7125 adv7123 Show More