Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC Quiz AQQ299 about Opamp open looop gain and LTspice (a kind proposal from Al Butvidas)

      1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits next to you and says 'wasn't that...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Understanding Voltage Domain Isolation in Field-Bus...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    PSM Integration for Enhanced Module Solutions in 48 V Data Centers

    The integration of the LTC2971 into quarter brick solutions for 48 V data centers enhances monitoring, control, and reliability by providing high precision...

EngineerZone
EngineerZone
High-Speed DACs
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
High-Speed DACs
  • Data Converters
High-Speed DACs
Documents ADV7123: Analog O/P values
  • Q&A
  • File Uploads
  • FAQs/Docs
  • Members
  • Tags
  • Cancel

Products Mentioned

ADV7123 Production
The ADV7123 (ADV®) is a triple high speed, digital-to-analog converter on a single monolithic chip. It consists of three high speed, 10-bit, video DACs...
Datasheet
ADV7123 on Analog.com

AD1580 Production
The AD1580 is a low cost, 2-terminal (shunt), precision band gap reference. It provides an accurate 1.225 V output for input currents between 50 μA and...
Datasheet
AD1580 on Analog.com

Table of Contents
  • HIGH-SPEED DAC SUPPORT COMMUNITY
  • +Documents
  • +AD768ARZ: FAQ
  • +AD9102: FAQ
  • +AD9106: FAQ
  • +AD9115: FAQ
  • +AD9116: FAQ
  • +AD9117: FAQ
  • +AD9119: FAQ
  • +AD9122: FAQ
  • +AD9129: FAQ
  • +AD9135: FAQ
  • +AD9142A: FAQ
  • +AD9144: FAQ
  • +AD9146: FAQ
  • +AD9148: FAQ
  • +AD9286: FAQ
  • +AD9712: FAQ
  • +AD9716: FAQ
  • +AD9717: FAQ
  • +AD9726: FAQ
  • +AD9734: FAQ
  • +AD9736: FAQ
  • +AD9739: FAQ
  • +AD9739A: FAQ
  • +AD9742: FAQ
  • +AD9744: FAQ
  • +AD9747: FAQ
  • +AD9748: FAQ
  • +AD974: FAQ
  • +AD9763: FAQ
  • +AD9765: FAQ
  • +AD9767:FAQ
  • +AD976A: FAQ
  • +AD9774: FAQ
  • +AD9776: FAQ
  • +AD9777: FAQ
  • +AD9779: FAQ
  • +AD9779A: FAQ
  • +AD977: FAQ
  • +AD977A: FAQ
  • +AD9780: FAQ
  • +AD9783: FAQ
  • +AD9786: FAQ
  • +AD9788: FAQ
  • +AD9789: FAQ
  • +AD9161: FAQ
  • +AD9162: FAQ
  • +AD9164: FAQ
  • +AD9856: FAQ
  • +AD9857: FAQ
  • +AD9957: FAQ
  • -ADV7123: FAQ
    • ADV7123 - Vref minimum and maximum specification is missing in the datasheet
    • ADV7123 EVB
    • ADV7123: Analog O/P values
    • ADV7123: Driving terminated video lines
    • ADV7123: Output with no power applied
  • +ADV7125: FAQ
  • +DPG3: FAQ
  • +MAX5189BEEI+: FAQ
  • +MAX5190BEEG+: FAQ
  • +MAX5868: FAQ
  • +MAX5871EXE+T: FAQ
  • +MAX5877EGK+D: FAQ
  • +MAX5880AUXF+: FAQ
  • +MAX5884EGM: FAQ
  • +MAX5891EGK+D: FAQ
  • +AD9136: FAQ
  • +AD9177: FAQ

ADV7123: Analog O/P values

Question

I have a question regarding the ADV7123 Video DAC. I connected the chip as
described in the datasheet with a 562 Ohm resistor on the RSET pin and SYNCN
(Sync on Green) to GND via a pull-down resistor. My test design is a rectangle
(should be gray) with a dark gray border and a thin white line (one pixel) on
the edge of the screen.
I can see what I would like to show but the colors are not correct since the
green signal (all three outputs with a 75 Ohm resistor to GND) has a larger
peak-to-peak signal than blue and red, although they are the same level. Any
Ideas? Could my voltage reference cause that? What happens if that voltage
reference drops below 1.25V?

Answer

The Rset value should be 530 Ohm, we don't recommend operating below this
value.

We have seen that when customers are operating the ADV7123 at high speed along
with rapid black/white transitions, an external reference such as the AD1580
should be used.

The internal ref at 5V is given in the datasheet.
We don't have a min and max spec for the internal ref at 3.3V, however we would
expect similar performance as the 5V spec's.

* To summatise, the max value for Rset should not exceed 530ohms for specified
performance.

* Using the part at high speeds and rapid black/white changes, places a high
current demand on the ADV7123 which affects the accuracy of the internal
reference. We have found that using a larger cap on Vref (i.e 4.4Uf)may allow
you to use the internal ref in this application, however we recommend using an
external ref.

* In order to achieve tight fullscale matching between parts, we recommend the
use of an external reference.

Tags: Standard High Speed D/A Converters high-speed dacs Shunt Voltage References 5D1N5844 High Speed D/A Converters =30MSPS voltage references ad1580 adv7123 Show More