Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC's Quiz AQQ298 about an interlaced square and triangle puzzle

      1. Quote of the month: " Behind every great man is a woman rolling her eyes " - Jim Carrey 2. New quiz AQQ298 about an interlaced square and triangle...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: ISO 26262 Essentials: Ensuring Confidence in Your Software...
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
    A Systematic Checklist for RF Transceiver Testing

    RF transceiver bring-up is the initial process of powering, configuring, and verifying a transceiver on new hardware to ensure basic functionality and...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Phase Sync in Digital Phased Arrays Through Direct RF SamplingPart 1: The Basics

    This article presents a methodology to synchronize multiple modular circuit boards, equipped with high speed data converters, to build a concept of a scalable...

EngineerZone
EngineerZone
High-Speed DACs
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
High-Speed DACs
  • Data Converters
High-Speed DACs
Documents Why is the interface 16-bits and the DAC 14-bits in the MAX5868?
  • Q&A
  • File Uploads
  • FAQs/Docs
  • Members
  • Tags
  • Cancel

Products Mentioned

MAX5868 Not Recommended for New Designs
The MAX5868 high-performance interpolating and modulating 16-bit 5Gsps RF DAC can directly synthesize up to 500MHz of instantaneous bandwidth from DC to...
Datasheet
MAX5868 on Analog.com

Table of Contents
  • HIGH-SPEED DAC SUPPORT COMMUNITY
  • +Documents
  • +AD768ARZ: FAQ
  • +AD9102: FAQ
  • +AD9106: FAQ
  • +AD9115: FAQ
  • +AD9116: FAQ
  • +AD9117: FAQ
  • +AD9119: FAQ
  • +AD9122: FAQ
  • +AD9129: FAQ
  • +AD9135: FAQ
  • +AD9142A: FAQ
  • +AD9144: FAQ
  • +AD9146: FAQ
  • +AD9148: FAQ
  • +AD9286: FAQ
  • +AD9712: FAQ
  • +AD9716: FAQ
  • +AD9717: FAQ
  • +AD9726: FAQ
  • +AD9734: FAQ
  • +AD9736: FAQ
  • +AD9739: FAQ
  • +AD9739A: FAQ
  • +AD9742: FAQ
  • +AD9744: FAQ
  • +AD9747: FAQ
  • +AD9748: FAQ
  • +AD974: FAQ
  • +AD9763: FAQ
  • +AD9765: FAQ
  • +AD9767:FAQ
  • +AD976A: FAQ
  • +AD9774: FAQ
  • +AD9776: FAQ
  • +AD9777: FAQ
  • +AD9779: FAQ
  • +AD9779A: FAQ
  • +AD977: FAQ
  • +AD977A: FAQ
  • +AD9780: FAQ
  • +AD9783: FAQ
  • +AD9786: FAQ
  • +AD9788: FAQ
  • +AD9789: FAQ
  • +AD9161: FAQ
  • +AD9162: FAQ
  • +AD9164: FAQ
  • +AD9856: FAQ
  • +AD9857: FAQ
  • +AD9957: FAQ
  • +ADV7123: FAQ
  • +ADV7125: FAQ
  • +DPG3: FAQ
  • +MAX5189BEEI+: FAQ
  • +MAX5190BEEG+: FAQ
  • -MAX5868: FAQ
    • Why is the interface 16-bits and the DAC 14-bits in the MAX5868?
  • +MAX5871EXE+T: FAQ
  • +MAX5877EGK+D: FAQ
  • +MAX5880AUXF+: FAQ
  • +MAX5884EGM: FAQ
  • +MAX5891EGK+D: FAQ
  • +AD9136: FAQ
  • +AD9177: FAQ

Why is the interface 16-bits and the DAC 14-bits in the MAX5868?

The noise floor in the system is determined by both quantization noise and thermal noise. The interface is 16-bits to ensure the DAC noise floor is dominated by thermal noise instead of quantization noise.  If the interface were only 14-bits, the quantization noise would increase and adversely affect the performance of the DAC as it would start to dominate the thermal noise.
Tags: MAX5868 000098085 high-speed dacs High Speed D/A Converters =30MSPS Fast Precision D/A Converters
  • Share
  • History
  • Cancel
 
Related Content
  • RE: Is there a maximum limit for A to D signal
    ADIApproved
    Hi Maria, There is a limit beyond which increasing the number of ADC bits (which reduces quantization noise) will not improve performance. It depends on the presence of other noise sources and if these...
  • RE: AD7768 Noise Floor
    JellenieR
    Yes for high resolution ADCs such as Sigma Delta ADCs the quantization noise is insignificant due to its inherently oversampling technique. So the ADC noise is primarily dominated by input reffered noise...
  • RE: DAC Noise Performance
    ADIApproved
    There are three main contributors in the DAC output noise. 1. Quantization noise. 2. DAC Clock wideband noise. 3. Noise from the current source array. Typically, at low output frequencies the current...
 
Related Content
  • RE: Is there a maximum limit for A to D signal
    ADIApproved
    Hi Maria, There is a limit beyond which increasing the number of ADC bits (which reduces quantization noise) will not improve performance. It depends on the presence of other noise sources and if these...
  • RE: AD7768 Noise Floor
    JellenieR
    Yes for high resolution ADCs such as Sigma Delta ADCs the quantization noise is insignificant due to its inherently oversampling technique. So the ADC noise is primarily dominated by input reffered noise...
  • RE: DAC Noise Performance
    ADIApproved
    There are three main contributors in the DAC output noise. 1. Quantization noise. 2. DAC Clock wideband noise. 3. Noise from the current source array. Typically, at low output frequencies the current...