Hello there,
I have been dealing with bringing up AD9152 with Xilinx FPGA JESD Tx Core with JESD PHY.
Followed all the guildelines through the datasheet of AD9152 but somehow link is getting down after passing to USERDATA state following CGS and ILAS states.
As the CGS and ILAS pass, the SPI register contents tell me that the lane are synced and locked but after ~3000 cycles from the first initilaization the link goes down.
Then the initilization loop began and goes continously. I am monitoring the SYNC pin that AD9152 drives for FPGA and it is toggling in a really frequent way.
Below I will give my parameters and a screenshot of Sync signal. I am stuck with the bringing up process. Any advice will be helpful.
Thanks in advance,
Berk
I am using custom board by the way and the lanes are well matched to 100ohm differential impedance and lane lengths are in between 17mm-20mm.
Try to get the Lane Rate of 8Gbps with the DAC RefClk of 200Mhz, FPGA MGT Ref CLK of 200Mhz and JESD Tx Core Clock as 200Mhz, all fed from HMC7044.
Trying to align first JESD204B Subclass0 therefore no SYS_REF included yet.
No lane swapping or lane polarity changes done on the board.
JESD PARAMETERS F=1 L = 4 M=2 K=32 S=1 N=16 N'=16 HD=1 which is JESD Mode 4 of AD9152.
DAC VCO is set 6.4Ghz and DAC Clock is 800Mhz which implies 8Gbps of line rate.
Below are the AD9152 Parameters :
parameters are given as 16bit address & 8 bit data
/* ========================================================================= */
/* 1. SPI & Device Verification */
/* ========================================================================= */
assign AD9152_ROM[0] = 24'h0000_81; /* Assert Reset */
assign AD9152_ROM[1] = 24'h0000_00; /* Deassert Reset */
assign AD9152_ROM[2] = 24'h0011_00; /* Enable DACs */
assign AD9152_ROM[3] = 24'h0080_04; /* Duty Enable */
assign AD9152_ROM[4] = 24'h0081_04; /* SYSREF Enable */
assign AD9152_ROM[5] = 24'h01CD_D8; /* Bandgap */
/* ========================================================================= */
/* 2. SERDES PLL/
/* ========================================================================= */
assign AD9152_ROM[6] = 24'h0284_62; /* ADI MUST WRITE */
assign AD9152_ROM[7] = 24'h0285_C9; /* ADI MUST WRITE */
assign AD9152_ROM[8] = 24'h0286_0E; /* ADI MUST WRITE */
assign AD9152_ROM[9] = 24'h0287_12; /* ADI MUST WRITE */
assign AD9152_ROM[10] = 24'h028A_2B; /* TABLE 36 */
assign AD9152_ROM[11] = 24'h028B_00; /* ADI MUST WRITE */
assign AD9152_ROM[12] = 24'h0290_89; /* ADI MUST WRITE */
assign AD9152_ROM[13] = 24'h0291_4C; /* TABLE 36 */
assign AD9152_ROM[14] = 24'h0294_24; /* ADI MUST WRITE */
assign AD9152_ROM[15] = 24'h0296_03; /* TABLE 36 */
assign AD9152_ROM[16] = 24'h0297_0D; /* ADI MUST WRITE */
assign AD9152_ROM[17] = 24'h0299_02; /* ADI MUST WRITE */
assign AD9152_ROM[18] = 24'h029A_8E; /* ADI MUST WRITE */
assign AD9152_ROM[19] = 24'h029C_2A; /* ADI MUST WRITE */
assign AD9152_ROM[20] = 24'h029F_7E; /* ADI MUST WRITE */
assign AD9152_ROM[21] = 24'h02A0_06; /* ADI MUST WRITE */
/* ========================================================================= */
/* 2. DAC PLL/
/* ========================================================================= */
assign AD9152_ROM[22] = 24'h008D_7B; /* ADI MUST WRITE */
assign AD9152_ROM[23] = 24'h01B0_00; /* ADI MUST WRITE */
assign AD9152_ROM[24] = 24'h01B9_24; /* ADI MUST WRITE */
assign AD9152_ROM[25] = 24'h01BC_0D; /* ADI MUST WRITE */
assign AD9152_ROM[26] = 24'h01BE_02; /* ADI MUST WRITE */
assign AD9152_ROM[27] = 24'h01BF_8E; /* ADI MUST WRITE */
assign AD9152_ROM[28] = 24'h01C0_2A; /* ADI MUST WRITE */
assign AD9152_ROM[29] = 24'h01C4_7E; /* ADI MUST WRITE */
assign AD9152_ROM[30] = 24'h01C1_2C; /* ADI MUST WRITE */
/* ========================================================================= */
/* 2. Optional DAC PLL/
/* ========================================================================= */
assign AD9152_ROM[31] = 24'h008B_02; /* ADI MUST WRITE */
assign AD9152_ROM[32] = 24'h008C_02; /* ADI MUST WRITE */
assign AD9152_ROM[33] = 24'h0085_08; /* ADI MUST WRITE */
assign AD9152_ROM[34] = 24'h01B6_49; /* Table 73 */
assign AD9152_ROM[35] = 24'h01B5_C7; /* Table 73 */
assign AD9152_ROM[36] = 24'h01BB_1A; /* Table 73 */
assign AD9152_ROM[37] = 24'h01B4_78; /* ADI MUST WRITE */
assign AD9152_ROM[38] = 24'h01C5_08; /* Table 73 */
assign AD9152_ROM[39] = 24'h008A_12; /* ADI MUST WRITE */
assign AD9152_ROM[40] = 24'h0087_62; /* ADI MUST WRITE */
assign AD9152_ROM[41] = 24'h0088_C9; /* ADI MUST WRITE */
assign AD9152_ROM[42] = 24'h0089_0E; /* ADI MUST WRITE */
assign AD9152_ROM[43] = 24'h0083_10; /* ADI MUST WRITE */ //--- READ PLL LOCK From 0x84
assign AD9152_ROM[44] = 24'h0083_90; /* ADI MUST WRITE */ //--- READ PLL LOCK From 0x84
//assign AD9152_ROM[44] = 24'h0083_10; /* ADI MUST WRITE */ //--- READ PLL LOCK From 0x84
/* ========================================================================= */
/* 2. DIGITAL DATA PATH/
/* ========================================================================= */
assign AD9152_ROM[45] = 24'h0112_00; /* ADI MUST WRITE */
assign AD9152_ROM[46] = 24'h0110_00; /* ADI MUST WRITE */
/* ========================================================================= */
/* 2. TRANSPORT LAYER/ JESD MOD 4
/* ========================================================================= */
assign AD9152_ROM[47] = 24'h0200_00; /* ADI MUST WRITE */
assign AD9152_ROM[48] = 24'h0201_00; /* ADI MUST WRITE */
assign AD9152_ROM[49] = 24'h0300_00; /* Checksum mode */
assign AD9152_ROM[50] = 24'h0450_49; /* DIDS */
assign AD9152_ROM[51] = 24'h0451_07; /* BIDS */
assign AD9152_ROM[52] = 24'h0452_00; /* LIDS */
assign AD9152_ROM[53] = 24'h0453_03; /* lane number & scrambling */ //SCRAMBLING OFF
assign AD9152_ROM[54] = 24'h0454_00; /* F-1 */
assign AD9152_ROM[55] = 24'h0455_1F; /* K-1 */
assign AD9152_ROM[56] = 24'h0456_01; /* M-1 */
assign AD9152_ROM[57] = 24'h0457_0F; /* N-1 */
assign AD9152_ROM[58] = 24'h0458_0F; /* Subclass & Np-1 */
assign AD9152_ROM[59] = 24'h0459_20; /* S-1 */
assign AD9152_ROM[60] = 24'h045A_80; /* ADI MUST WRITE */
assign AD9152_ROM[61] = 24'h046C_0F; /* ADI MUST WRITE */
assign AD9152_ROM[62] = 24'h0476_01; /* ADI MUST WRITE */
assign AD9152_ROM[63] = 24'h047D_0F; /* ADI MUST WRITE */
/* ========================================================================= */
/* 2. PHYSICAL LAYER/
/* ========================================================================= */
assign AD9152_ROM[64] = 24'h02AA_B7; /* ADI MUST WRITE */
assign AD9152_ROM[65] = 24'h02AB_87; /* ADI MUST WRITE */
assign AD9152_ROM[66] = 24'h02A7_01; /* ADI MUST WRITE */
assign AD9152_ROM[67] = 24'h0314_01; /* ADI MUST WRITE */
assign AD9152_ROM[68] = 24'h0230_29; /* ADI MUST WRITE */
assign AD9152_ROM[69] = 24'h0206_00; /* ADI MUST WRITE */
assign AD9152_ROM[70] = 24'h0206_01; /* ADI MUST WRITE */
assign AD9152_ROM[71] = 24'h0289_04; /* ADI MUST WRITE */
assign AD9152_ROM[72] = 24'h0280_01; /* ADI MUST WRITE */
assign AD9152_ROM[73] = 24'h0280_05; /* ADI MUST WRITE */
assign AD9152_ROM[74] = 24'h0268_62; /* ADI MUST WRITE */
/* ========================================================================= */
/* 2. DATALINK LAYER/
/* ========================================================================= */
assign AD9152_ROM[75] = 24'h0301_00; /* ADI MUST WRITE */
assign AD9152_ROM[76] = 24'h0304_04; /* LMFC Delay */
assign AD9152_ROM[77] = 24'h0306_0A; /* LMFC Buffer */
assign AD9152_ROM[78] = 24'h003A_01; /* ADI MUST WRITE */
assign AD9152_ROM[79] = 24'h003A_81; /* ADI MUST WRITE */
assign AD9152_ROM[80] = 24'h003A_C1; /* ADI MUST WRITE */
assign AD9152_ROM[81] = 24'h0308_08; /* lane mapping */
assign AD9152_ROM[82] = 24'h0309_1A; /* lane mapping */
assign AD9152_ROM[83] = 24'h0334_00; /* polarity reversal */
assign AD9152_ROM[84] = 24'h0034_07; /* error window */
assign AD9152_ROM[85] = 24'h0300_01; /* ADI MUST WRITE */
By the way, the SERDES PLL and DAC PLL is always seems to be LOCK which is read from 0x084 and 0x281 register.
This is the Xilinx JESD TX core parameters
parameters are as 8 bit address & 32 bit data
assign JESD204_ROM[0] = 40'h20_00000001; /* Assert Reset */
assign JESD204_ROM[1] = 40'h24_00000002; /* CTRL ENABLE */
assign JESD204_ROM[2] = 40'h34_00000000; /* SubClass */
assign JESD204_ROM[3] = 40'h3C_030E1F00; /* Lane Params */ // SCRAMBLING OFF
assign JESD204_ROM[4] = 40'h70_00000749; /* BID & DID */
assign JESD204_ROM[5] = 40'h74_000F0F01; /* Lane Params */
assign JESD204_ROM[6] = 40'h78_00010000; /* Lane Params */
assign JESD204_ROM[7] = 40'h40_0000000F; /* Lane Enable */
assign JESD204_ROM[8] = 40'h48_00000000; /* Test Mode */
assign JESD204_ROM[9] = 40'h20_00000000; /* Desssert Reset */
Edit Notes
AD9152 is added to title[edited by: berkbasaklar at 4:48 PM (GMT -4) on 27 Oct 2026]