Post Go back to editing

AD9154-FMC-EBZ: digital sample code to output voltage?

Category: Hardware
Product Number: AD9154

Hi, I am using AD9154-FMC-EBZ board, driven by FPGA (ZCU102) logic.

Could you please let me know the relationship between the 16-bit input sample to DAC and the voltage measured at the analog output connector?

AD9154 is a current-output DAC

full-scale current & DAC digital gain are set to maximum values.

Thanks

  • Hi  ,

    Thank you for using AD9154.

    The 16-bit input sample controls the differential output current, not the output voltage directly. With maximum DAC gain, the full-scale output current is approximately 20 mA.

    The AD9154 itself produces current, so the voltage measured at the AD9154-FMC-EBZ connector is determined by the board's output termination/transformer network:



    where DACCODE = 0 to 2N − 1 and is the digital signal input to a DAC core consisting of a stream of 16-bit samples.

    Therefore, the digital-code-to-current relationship comes directly from the DAC, while the current-to-voltage relationship must include the AD9154-FMC-EBZ output circuit.

    Thanks and kind regards,

    Alex

  • Hi  

    Thank you for your reply

    Could you please let me know "the current-to-voltage relationship must include the AD9154-FMC-EBZ output circuit."?

    Thanks

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.