Post Go back to editing

Is AD9783 Monotonic

Thread Summary

The user asked if the AD9783 is monotonic, given the ±2 LSB DNL specification. The final answer confirms that the AD9783 is guaranteed to be monotonic, and the ±2 LSB DNL is a linearity/accuracy metric, not an indication of non-monotonicity. The 'Main DAC Monotonicity Guaranteed' specification in Table 1 applies to all AD978x parts.
AI Generated Content
Category: Datasheet/Specs
Product Number: AD9783

Is the AD9783 Monotonic? The datasheet stays the DNL is +/-2 LSB which would make me think not. However, in Table 1, under 'Main Outputs' is a line: 'Main DAC Monotonicity Guaranteed' but that's the label for the row that is empty to right, so it that just a category or is it describing the behavior of the AD978X including the AD9783?

Thank you,

Ben

  • Hi  ,

    Thanks for reaching out with your question

    Yes, the AD9783 is guaranteed monotonic.

    The line in Table 1 — “Main DAC Monotonicity Guaranteed” — is an actual specification that applies to all AD978x parts, including the AD9783.

    The ±2‑LSB DNL figure in the datasheet doesn’t indicate non‑monotonicity; for this high‑speed DAC, it represents a general linearity/accuracy metric used for system modeling.

    Thanks and kind regards,

    Alex

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.