Post Go back to editing

Data Sheet inconsistency

Thread Summary

The user asked about inconsistencies in the AD9776A DAC Rev C data sheet, specifically regarding the DATACLK Delay Mode bit (Register 3, Bit 7) and the reserved bit (Register 3, Bit 6). The final answer confirmed that Bit 7 is the DATACLK Delay Mode bit (0: Manual, 1: Automatic) and should be set to 1 for automatic delay adjustment. Bit 6 is reserved and should remain at 0. The DATACLK Delay is a 5-bit number, and setting Bit 7 to 1 enables constant timing margin checking and DATACLK Delay updates.
AI Generated Content
Category: Datasheet/Specs
Product Number: AD9776A

I have a couple questions regarding the Rev C data sheet of the AD9776a DAC. On page 28 register 3 bit 7 shows DATACLK Delay Mode. Page 30 describes this same bit as reserved set to 0.  I am guessing that this bit is really the DATACLK Delay Mode bit and that it can be set to a 1 and that setting this bit to a 1 allows the part to automatically determine the data clk delay needed to satisfy the data timing margin that is set in register 3 bits [3..0]. Is that correct???

Register 3 bit 6 is shown as reserved (set to 0) on page 28. Page 30 shows bit 6 as reserved and that it should always be set to a 1 with a default of 0.  I am guessing that since the default is 0 that bit 6 should always be set to a zero.  What should bit 6 in register 3 be set to??

Register 2 bit 4 is the DATACLK Delay enable bit. It says on page 29 that more details on this feature are discussed in the optimizing the data input timing section but DATACLK Delay enable bit isn't mentioned at all.  I assume that I should set this enable bit after I have the input reference clock set up and data is streaming to the part.  Is that correct??

In digital control register 1 I see a bit called DATACLK Delay [4]. I assume that this is the most significant bit of the DATACLK Delay bits [3..0] located in register 4 bits [7..4]. Figure 86 on page 48 shows that DATACLK Delay bits [3..0] is only 4 bits.  Is DATACLK Delay a 5 bit number?? 

The data sheet also states on page 48 

One error check operation
is performed per device configuration. Any change to the Data
Timing Margin[3:0] or DATACLK Delay[3:0] values triggers a
new error check operation.

if I set bit 7 of register 3 to a 1 (DATACLK Delay Mode = 1) Is the timing margin constantly checked and is the DATACLK Delay constantly updated?

Thanks 

Thread Notes

Parents
  • Hi  ,

    Thank you for bringing your concern regarding the AD9776A datasheet to our attention. We will review your queries and provide an update accordingly.

    Thanks and kind regards,

    Alex

  • Understood but can you answer some of the other questions like what should register 3 bit 6 be set to a 1 or 0?  Also can you answer the regarding how timing margin works??

    Register 3 bit 6 is shown as reserved (set to 0) on page 28. Page 30 shows bit 6 as reserved and that it should always be set to a 1 with a default of 0.  I am guessing that since the default is 0 that bit 6 should always be set to a zero.  What should bit 6 in register 3 be set to??

    The data sheet also states on page 48 

    One error check operation
    is performed per device configuration. Any change to the Data
    Timing Margin[3:0] or DATACLK Delay[3:0] values triggers a
    new error check operation.

    if I set bit 7 of register 3 to a 1 (DATACLK Delay Mode = 1) Is the timing margin constantly checked and is the DATACLK Delay constantly updated?

Reply
  • Understood but can you answer some of the other questions like what should register 3 bit 6 be set to a 1 or 0?  Also can you answer the regarding how timing margin works??

    Register 3 bit 6 is shown as reserved (set to 0) on page 28. Page 30 shows bit 6 as reserved and that it should always be set to a 1 with a default of 0.  I am guessing that since the default is 0 that bit 6 should always be set to a zero.  What should bit 6 in register 3 be set to??

    The data sheet also states on page 48 

    One error check operation
    is performed per device configuration. Any change to the Data
    Timing Margin[3:0] or DATACLK Delay[3:0] values triggers a
    new error check operation.

    if I set bit 7 of register 3 to a 1 (DATACLK Delay Mode = 1) Is the timing margin constantly checked and is the DATACLK Delay constantly updated?

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.