Hello,
I have been testing phase noise on the AD9142A for use in a noise critical application.
I get adequate results when generating a 100MHz tone using the DPG Lite pattern generator + SDP-H1 development board interfaced to the AD9142A...
But if I enable the AD9142A internal NCO the phase noise degrades substantially.
To do a one-to-one comparison I have two test configurations (both via the SDP-H1 running DPG Lite pattern to AD9142A):
- 100MHz pattern -> SDP-H1 -> LVDS -> AD9142A (no internal NCO)
- Static DC level -> SDP-H1 -> LVDS -> AD9142A with internal NCO at 100MHz
The results are as follows:

Is this expected behavior? Any way to mitigate?