Post Go back to editing

AD9744-FMC-EBZ-J3/J4 EXT REF/DAC CLK

Thread Summary

The user inquires about using the AD9744-FMC-EBZ with an external clock input in the 100 kHz to 500 kHz range. The AD9744 can handle low frequencies, but the RF transformer (TMC2-43X+) on the board restricts operation below 10 MHz. Removing the transformer and adding a buffer and coupling is suggested, and the SDP-H1 controller is not optimized for very low data rates, potentially limiting operation. The ACE and DPG Lite software can support low-frequency clocks.
AI Generated Content
Category: Hardware

Hello, 

I would like to confirm for AD9744-FMC-EBZ-J3 EXT REF/DAC CLK.

The AD9744-FMC-EBZ's onboard clock has a minimum speed of 40 MHz, but we received an inquiry from the customer about using an external clock input to operate at low frequencies of around 100 kHz to 500 kHz.

Could you please your opinion the below ?
-What is the supported frequency range for the external clock input?
(Not mentioned in the datasheet.)

-I would appreciate some advice on using it at frequencies between 100 kHz and 500 kHz.
The external clock input is equipped with an RF transformer (TMC2-43X+), so it is unlikely that frequencies below 10 MHz can be input. So, I think that modifications such as removing the RF transformer will be necessary. Are there any other functional issues?

Even if a clock compatible with the electrical characteristics of the AD9744 and the Spartan 6 on the SDP-H1 are input, I am concerned that there may be frequency limitations due to the SDP-H1, ACE software, DPG Lite software, or other design tools, which is why I would be confirmed this question.

  • Hi  ,

    Thank you for forwarding the customer’s queries to us.

    Using a low-frequency clock in the 100 kHz–500 kHz range is technically possible with the AD9744 IC but requires hardware modifications (removal of RF transformer and proper coupling), and software/FPGA validation to ensure the evaluation ecosystem doesn’t reject or alter the low clock input.

    Could you please share more details about the customer’s requirements or applications so we can evaluate other possible alternatives? Additionally, could you clarify why they selected the AD9744 for their application?

    Please find below additional details regarding your queries

    What is the supported frequency range for the external clock input?
    • From practical standpoint DAC can handle DC to 210 MSPS; however, we usually recommend getting a DAC with a sampling rate (FCLK) at least 4x the desired FOUT.

    The external clock input is equipped with an RF transformer (TMC2-43X+), so it is unlikely that frequencies below 10 MHz can be input. So, I think that modifications such as removing the RF transformer will be necessary. Are there any other functional issues?
    • You’re correct — the TCM2‑43X+ restricts operation below 10 MHz.
    • Remove transformer, add buffer and coupling; verify CMOS thresholds.
      • You can refer to "Figure 51. LFCSP Evaluation Board Schematic—Clock Input" of RevC datasheet.

    Even if a clock compatible with the electrical characteristics of the AD9744 and the Spartan 6 on the SDP-H1 are input, I am concerned that there may be frequency limitations due to the SDP-H1, ACE software, DPG Lite software, or other design tools, which is why I would be confirmed this question.
    • SDP-H1 is optimized for evaluating high-speed DACs, typically in the tens to hundreds of MSPS range.  As per our performed evaluation, it can support down to 10MHz only.  At present, we do not have a controller capable of operating at very low data rates due to limitations in both hardware and software architecture.
    • ACE & DPG Lite software can support low-frequency clock.

    Thanks and kind regards,

    Alex

  • Hello Alex-san,
    Thank you for your quick response.
    I haven't received a response regarding the customer's application yet, so I will send you a message once I receive one or if there is any further confirmation. First of all, thank you for your quick response.